Dear All,

 

I am using the Si4684 with firmware rev 26 (DAB 5.0.5).

 

In the datasheet it states the feature

 

* Concurrent I2S / L-R stereo audio out

 

However, this doesn't appear to be the case, I can have either L-R or I2S but not both.

My I2S is configures as MASTER, 48kHz. 

 

If I set PIN_CONFIG_ENABLE to 0x8002, then I get I2S output OK.

If I set PIN_CONFIG_ENABLE to 0x8001, then I get L-R output OK

 

but If I set PIN_CONFIG_ENABLE to 0x8003, then I only get L-R and No I2S DOUT (it is low). 

Note that FS and CLK are working with 0x8003 setting.

 

(I'm rebooting between changes - so it is not that there isn't a tune to set up the settings).

 

I've also tried in I2S SLAVE mode, and the same is true, DOUT only works with PIN_CONFIG_ENABLE set to 0x8002.

 

Anybody got concurrent I2S and L-R with Si4684 ? or have any ideas why I'm not !

 

Sincerely,

Adrian

 

  • Audio and Radio
  • Discussion Forums
  • Answered
Answered
  • hi

    it is only I2S or L-R can be enabled at a time. If both enabled, only analog audio output is enabled. do you need to enable both mode at a time in your system? 

    Correct Answer
    0
  • Dear clzhan,

     

    Thank you, No I don't really need both at the same time, but the datasheet suggests that you can, and I wondered whether I was missing the trick.

     

    Sincerely,

    Adrian

     

    0
  • I see, what kind of produce you are development  and how it going on 

     

    best regards

    clzhan

    0