Hi!, I have a setup with a PIC24FV16KM202 and a Si4703 in I2C mode. 

If I touch any of the pin's at the Si4703 breakout board the music stop's and the frequency is changed to 87,5MHz??

In my search I have soldered 1uF at the +3.3v and gnd, and I still have the issue.

 

Thank you for your time. 

  • Audio and Radio
  • Discussion Forums
  • Answered
Answered
  • Hi Elmek,

     

    The host MCU may be reset when you touch the wire. 
    Can you check the voltage of the power supply when you touch the wire?

    0
  • Hello,

     

    Please have a try of the circuit in attached file. The RC circuit(resistor and cap) need to be placed very close to the pin5 of the tuner.

     

    Regards

     

    Mingliang Yang

    Correct Answer
    0
  • Hello, thank you for the answer.
    That works, now there is no problem when touching Any of the pins.
    Regards Michael Hinsch Nedergaard
    0