Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Chapter 10.1: Control an accelerometer over I2C Part 1 - Connect the breakout board

03/62/2016 | 02:53 PM
lynchtron

Level 5


10_i2c_teaser.jpg

In this chapter, we will learn how to use the I2C bus to configure and read the live acceleration data from an accelerometer.  We will connect the circuit to your Starter Kit, create interface code, and then output the measurement data over a serial port to your computer in real time.  We will then create an interrupt routine to detect a “freefall” event to trigger an LED on the Starter Kit.

 

This chapter aims to first teach how to connect to an I2C device with the help of the EFM32 I2C library.   I2C is a commonly utilized communication interface for embedded designs.  Thanks to only requiring two pins on the MCU, plus the fact that many devices can connect over those two pins makes it very versatile.  In order to give us an interesting I2C device to talk to on the other end of that bus, I chose an accelerometer.

 

An accelerometer is a device that can measure acceleration on one or more axes.  It can be used to detect the orientation of your device relative to the earth’s gravity.  This can be useful for tilt sensors, to tell your object if it is right-side up, or upside-down.  But they can also measure acceleration due to movement, which would be good know if your device needs to know how it is moving through space.  And it doesn’t just tell you that it is moving, but how much it is accelerating, and in which direction even if that means that there is no acceleration on your device at all, as in a free fall situation.  That information could be helpful if your device is delicate needs to prepare itself for a hard landing!

 

Accelerometers are a relatively new invention available to electronics developers.  Long ago, an accelerometer was a large mechanical device that contained springs and plates.  They were heavy, large, and expensive.  That has changed for two reasons 1) Miniaturization of the mechanical parts of an accelerometer has shrunk it down to fit on a single surface-mounted chip and 2) they are employed in smart phones the world over, which drives down the cost for the rest of us.

 

Materials Needed for This Lesson

  • ADXL345 Breakout Board
  • Soldering iron and solder
  • Jumper wires

Accelerometer Theory

Modern accelerometers are Micro Electro-Mechanical Systems (MEMS) devices, which means that they are able to fit on a small chip inside the smallest of gadgets.  One method to measure acceleration employed by MEMS accelerometers is to utilize a tiny conductive mass suspended on springs.  The acceleration of the device causes the springs to stretch or contract, and the deflection of the conductive mass can be measured through a change in capacitance to nearby, fixed plates. 

 

Accelerometers are specified by the following features:

  • The number of axes, from one to three axes, labeled X, Y, and Z in the specification diagrams. Note that some accelerometers are called 6-axis or 9-axis, but that just means that they are bundled with other MEMS devices such as gyroscopes and/or magnetometers.  Each of those devices also have three axes, which is why there are 3, 6, or 9-axis Inertial Measurement Units (IMUs).
  • The type of output, either analog or digital. An analog accelerometer outputs a voltage to indicate the acceleration on a particular axis and would require an Analog-to-Digital Converter (ADC) or Analog Comparator (ACMP) pin on the MCU to make sense of the data.  Both of these types of pins exist in the EFM32 family.  A digital accelerometer takes care of formatting the acceleration data into a digital representation that can be read out over I2C or SPI.
  • The range of acceleration measured in g’s, where 1g is the acceleration due to Earth’s gravity.
  • The resolution, or update frequency, measured in Hertz (Hz). Some accelerometers can be used to analyze very fast, dynamic events such as a golf swing, while others can only be used to detect the static tilt angle of your gadget.
  • Coprocessors that can offload some of the calculations needed to analyze the raw data from the MCU. Most accelerometers have some simple interrupt capability to detect an acceleration threshold (shock) and a 0-g (freefall) condition.  Others can do advanced processing on the raw data to offer more meaningful data to the MCU.

10.1_axes.png
Axes of the ADXL345 Accelerometer

The ADXL345 accelerometer used in this lesson is a digital output accelerometer that has three axes and a selectable g-range of 2/4/8/16 g’s.  It connects to the MCU using an I2C or SPI interface.  Note that we are going to demonstrate the I2C bus for this lesson, but I2C limits the measurement frequency to 800Hz whereas SPI allows a higher frequency of 1600Hz.  Keep that in mind if your application requires the higher frequency.

 

Connect the Accelerometer to the Starter Kit via I2C

The I2C bus is a shared bus that consists of only two signals, a clock line (SCL) and a data line (SDA).  A single I2C bus can connect two or more devices and any device can be a master or a slave (the same device can even assume both roles at different times).  Only masters can initiate communication.  Slave devices are assigned unique 7-bit or 10-bit device addresses through hardware configuration and monitor the bus for their address to be called, responding to any master device that begins a transaction.  That means that you have to ensure that each slave device on your I2C bus has a unique address. 

 

10.1_diagram.png

 

An I2C bus requires pull-ups on the SDA and SCL lines to keep the bus at a high voltage level when neither the master nor slave device is driving the bus.  The pull-ups are created by attaching each of the interface wires to the supply voltage through an appropriately-sized resistor.  The size of the resistor is chosen by the length of trace that will be used, which impacts the capacitance of the trace, and the speed of the I2C bus.  Long traces create higher capacitance and require a lower value resistor to return the wire to a high voltage level after an I2C device has stopped driving the wire to a low voltage level. 

More information can be found about I2C by viewing the official specification here.  Sparkfun has a good tutorial here, and there’s another good tutorial from Robot Electronics here.


Your ADXL345 breakout board is shipped without header pins attached.  You have to solder them to the board as was demonstrated in Lesson 4, where we did the same thing to our Starter Kit.
 10.1_breakout.png
In order to connect the accelerometer to the Starter Kit via the I2C bus, I had to figure out which pins were available on the Starter Kit that were connected to an I2C peripheral inside the Wonder Gecko MCU.  I started with the Datasheet for the Wonder Gecko, which I found in the tile view in the Simplicity Studio home page.  I then looked to section 4.2 Alternate Functionality Pinout and found the available I2C interfaces and locations where those interfaces routed to GPIO pins.

10.1__gpios.png

I found that the location 0 on I2C0 was not available on the Starter Kit, but the second one was available.  I connected PD7 to the SCL pin on the ADXL345 breakout board and connected PD6 to the SDA pin on the breakout board.  I then connected 3V3 on the Starter Kit to the VIN pin on the ADXL345 breakout board.  I then placed a wire between GND pins on each board.

 

NOTE: The 3V3 pin on the ADXL345 breakout board is an output pin to power other devices, not an input pin for the board.  The input pin is labeled as VIN. 

10.1_connections.png
Note that you could have built your own breakout board if you wanted to use an I2C device that had no breakout board or evaluation board available.  Follow the instructions in Lesson 9, where a flash chip was given a breakout board with the help of a blank Schmartboard breakout board. 

 

In the next section, we will cover software configuration of the I2C interface on the MCU for the ADXL345 accelerometer.

 

PREVIOUS | NEXT

  • Blog Posts
  • Makers

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • IoT Hero CoreTigo Drives New Wireless Standard...
  • A Guide to IoT Protocols at Works With...