Silicon Labs Silicon Labs Community
silabs.com
Language
  • 简体中文
  • 日本語
  • MCUs
    • 8-bit MCU
    • 32-bit MCU
  • Wireless
    • Bluetooth
    • Proprietary
    • Wi-Fi
    • Zigbee & Thread
    • Z-Wave
  • More Products
    • Interface
    • Isolation
    • Power
    • Sensors
    • Timing
  • Development Tools
    • Simplicity Studio
    • Third Party Tools
    • Thunderboard
  • Expert's Corner
    • Announcements
    • Blog
    • General Interest
    • Projects
  1. Community - Silicon Labs
  2. Blog

Sense Makes Everything: Introducing the Thunderboard Sense Inspiration Kit

09/272/2016 | 08:48 PM
Lance Looper
Employee

Level 5


IoT development is happening at a breakneck pace, with consumer demand driving pressure to get connected products to market quickly. But getting into the hands of consumers is only part of the challenge, these products need to work pretty much as-expected. Creating a positive user experience is critical for any emerging technology and IoT is no different. Great products drive demand, and demand drives innovation. Rinse and repeat.

 

One of our goals is to help developers get to market quickly, but to also make great tools available that demonstrate the speed and effectiveness with which IoT connectivity can be achieved. This is why we’ve created the Thunderboard development platform.

 

Over the summer we unveiled Thunderboard React, which we designed as a cost-effective prototyping vehicle to demonstrate how easy it can be to connect wireless sensor nodes to mobile devices and the cloud. It featured a battery-powered, sensor-rich demonstration board with a Bluetooth low-energy module based on an ARM Cortex-M4 CPU for IoT connectivity, plus open-source design files and software for mobile applications running on Android and iOS devices.

 
Thunderboard Sense Lable.png

Now we’re expanding the platform with the introduction of Thunderboard Sense. This addition to the Thunderboard family blazes new ground with a host of sophisticated sensor technology and support for not only Bluetooth low energy, but ZigBee, Thread and proprietary wireless protocols as well. To complete the picture, Thunderboard Sense is developer friendly.  Connect to Simplicity Studio and proceed to hack away, without any other debug or programming hardware needed.

 

Once users have the opportunity to work with the embedded and mobile apps that come ready to go out of the box, we think they’ll be inspired to ask “what else can I do?” The logical next step is to incorporate the Thunderboard Sense as-is into an end product to provide device-to-cloud functionality.

 

Users can also push the boundaries of the device by using the open source hardware design files and software source code to integrate portions of the Thunderboard React into other projects. And by modifying the firmware on the board itself, customers can program the Blue Gecko module using an adapter. 

 

Thunderboard Sense ships with a revamped mobile app (iOS and Android) so you can demonstrate cloud connected sensors within minutes of taking it out of the box. It also comes with a powerful, multi-protocol EFR32 Mighty Gecko radio, an integrated debugger and is fully supported in Simplicity Studio.

 

Thunderboard Sense.png

 

The Sense brings together the best of what Silicon Labs has to offer in a single, easily accessible prototyping kit. The radio and sensors have industry-leading power consumption and the firmware and mobile app have been developed specifically to capitalize on the power saving features of each device.

 

We can’t wait to see what you do with it! Get Started with Thunderboard Sense here.

 

 

  • Blog Posts
  • Internet of Things
  • josh1

    Level 3


    Replied Oct 20 2016, 3:38 PM

    I understand that this board just came out a month ago. However development resources have been scarce. Is there a timeline to add sample code to Simplicity Studio soon?

    0
  • airsharma

    Level 3


    Replied Oct 20 2016, 6:58 PM

    @josh1 Sample code for Thunderboard Sense is available in Simplicity Studio v4.  You can download this free tool at www.silabs.com/simplicity.  The software examples we offer are:

    • Blink
    • Blink RGB
    • Connected Motion (for 2.4GHz proprietary)
    • EMode
    • the "Official Thunderboard Sense App" (for BLE)
    • VCom
    • Empty BLE
    • NCP Empty target
    • SOC Empty
    • SOC Thermometer (for BLE)
    • SOC iBeacon (for BLE)

     

    0
  • josh1

    Level 3


    Replied Oct 20 2016, 8:36 PM

    @airsharma Thanks for the reply. It turns out that the Simplicity Studio I downloaded last week didn't have the sample code. I re-downloaded the Simplicity Studio and now I see all the Sense sample code. Thanks!

    0
  • edu69

    Level 3


    Replied Oct 28 2016, 1:32 PM

    Hi, I ordered and received two Senses last week. I´ve downloaded and installed Simplicity v4 in Windows10, but Simplicity doesn´t recognize any board by USB cable. What´s the problem? Is it necessary to install any other USB driver or something like that?

    Thanks in advance,

    Eduardo

    0
  • airsharma

    Level 3


    Replied Oct 28 2016, 1:41 PM

    @edu69

    Thanks for ordering Thunderboard Sense kits!  We include support for these kits via an update to Simplicity Studio in the "wireless" package.  I have 2 suggestions.  First, make sure that you install ALL of Simplicity Studio or if you don't want to do that due to disk space restrictions, make sure to install the wireless package.  See below:

     

     

    Picture1.png

     

    Then, after Simplicity Studio finishes the installtion and restarts, please click the update button  (shown by the white arrow) on the top toolbar.  See below.

     

    Picture1.png

     

     

    0
  • edu69

    Level 3


    Replied Oct 28 2016, 7:30 PM

    @airsharma Thanks for the quick answer.

    I installed all the families and devices, including Wireless Products. Referred to the second suggestion, I guess that I have to push the update button with the Sense board connected to the PC, anyway it doesn´t appear any message about JLink Silicon Labs under Device tab.

    Anotther check: If I connect the board to the PC (without launching Simplicity), a virtual COM port should appear in Windows Device Manager, shouldn´t it? But none virtual COM port appears. 

    The boards have the references below:

    Part Number: SLTB001A

    Date: 29-08-16

    Serial Number. 1635000211 and 1635000278

    Rev.: B00

    PCB4160A Rev A02

    The boards are exactly like the picture at the beginning of this article but with a small difference (my boards don´t include the Hall effect sensor soldered on the PCB, though the pads and the layout of the tracks seem to be completely routed to the microcontroller and other components).

    Any idea, please? Thanks again.

    0
  • airsharma

    Level 3


    Replied Nov 01 2016, 9:37 PM

    @edu69 If you're still having trouble, please send me your contact details at raman.sharma@silabs.com.  I'll try to walk you through the set-up process.

     

    0
  • ionu

    Level 3


    Replied Nov 10 2016, 6:55 PM

    When will the hall effect sensor be available on the board?

    0
  • airsharma

    Level 3


    Replied Nov 10 2016, 7:37 PM

    @ionu We are targeting Q1 2017 to build the next revision of the Thunderboard Sense.  This revision will inlcude the hall effect sensor.

    0
  • ionu

    Level 3


    Replied Nov 11 2016, 3:08 AM

    What would be needed ro test/eval a small thread network using this kit.

    WIll the BLE stack on this board be upgradable to BLE 5 when it arrives soon.

    0
  • 1
  • 2
Next

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32MG21 Series 2 SoCs
  • Blue Gecko Series 2
  • Zigbee SDK
  • ZigBee and Thread
  • Internet Infrastructure
  • Sensors
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Mighty Gecko SoCs
  • Timing
  • Blue Gecko Bluetooth Low Energy Modules
  • Clocks
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • blue-gecko-xpress-modules
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Isolation
  • Powered Devices

Top Authors

  • Avatar image Mark Mulrooney
  • Avatar image Siliconlabs
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2014 December
  • 2015 January
  • 2015 February
  • 2015 March
  • 2015 April
  • 2015 May
  • 2015 June
  • 2015 July
  • 2015 August
  • 2015 September
  • 2015 October
  • 2015 November
  • 2015 December
  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
Silicon Labs
  • About Us
  • In the News
  • Email Newsletter
  • Cookies
  • Contact Us
  • Community
  • Site Feedback
  • Investor Relations
  • Blog
  • Privacy and Terms
  • Corporate Citizenship
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号-1