Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Outstanding Performance by Silicon Labs’ Isolation in University Study

06/170/2017 | 02:00 PM
Lance Looper
Employee

Level 5


Recently, it was brought to my attention that Silicon Labs’ Isolators were part of a study at Aalto University in Finland. The study was conducted by Mikael Lumio as part of his Master’s program. The results are interesting and one of the most comprehensive, independent studies of isolation performance I have seen.

 

The full thesis is available here.

 factory-floor copy.jpg

 

Mr. Lumio approaches some of the concerns surrounding CMOS-based isolation straight on. In his thesis, he compares different types of CMOS isolation against each other and against the legacy optocoupler solutions. Capacitive-based isolators (the preferred technology from Silicon Labs), inductive (transformer)-based isolators, and magnetoresistive-based isolators are all included in the analysis. For many specs, the capacitive-based solutions outperform other technologies. Compared to optocouplers, Mr. Lumio’s analysis clearly shows advantages of CMOS-based isolation in common-mode transient immunity (CMTI), current consumption per channel, data rate, skew, and other timing specifications.

 

In addition to comparing datasheet specifications, Mr. Lumio also compares isolation performance. Mr. Lumio’s thesis does an excellent job of describing the different isolation parameters that are commonly specified by international certifying agencies. Then, the thesis uses those descriptions to aide in the comparison of different CMOS isolation technologies. For all technologies, the isolation capability is on par with legacy optocoupler devices. The only lagging parameter is in surge immunity, but CMOS-based isolators are catching up fast.

 

Mr. Lumio’s thesis is particularly focused on the application of isolation technology to variable frequency drive (VFD) systems. VFDs are increasingly used in all types of motor drive applications. Motor drive efficiency standards worldwide encourages the use of variable frequency drives wherever it is applicable to a motion application. The thesis lists, “blowers, compressors, conveyor belts, cooling and recirculating pumps, cranes, factory robotics, fans, elevators, hoists, mixers, paper mills, and printing presses,” as relevant applications where VFDs are prescribed for efficiency improvement.

 

VFDs are usually powered from rectified AC line inputs and are used to provide a three-phase, AC output to a motor. The supply provides a high DC voltage for the rest of the system. Isolation is necessary in several parts of the typical system. The VFD is converting the DC supply into an AC signal through a multi-phase inverter stage. The inverter has switches connected to the high voltage power rail and isolation must be utilized to protect the control circuit. The output of the drive is connected to the windings of the motor. Often each winding has an isolated sensor connected for current and voltage measurement. Both safety isolation, for protection of operators and people interfacing with the system, and functional isolation, for circuit protection, are necessary in the system.

 

Besides specific isolation requirements, Mr. Lumio looked at additional features of CMOS-based isolation to evaluate its suitability for use in VFDs. Electromagnetic compatibility (EMC) was of particular concern. ESD performance was also evaluated. Finally, the relative cost of the various CMOS isolators was considered.

 

On the subject of cost, the thesis found that at mass production volumes CMOS-based isolators are less expensive. In his analysis, Mr. Lumio included not only the device cost but also indirect costs including the reduction in PCB area and component count. For the typical fieldbus serial communication application, Mr. Lumio’s research indicates a close to 1/5 cost reduction in moving from a legacy optocoupler solution to a modern isolation solution. For a more specific IGBT drive function, the cost reduction wasn’t as large. It was still significant, though, at approximately 1/10.

 

EMC was a focus for Mr. Lumio’s thesis because of the environments in which VFDs operate. High voltage switching associated with motor drive means that the components used must be immune to a large amount of electromagnetic noise. Mr. Lumio found that modern CMOS-based isolators performed as expected even in the presence of large amounts of electromagnetic interference. Silicon Labs’ isolators showed great robustness in all test. For example, in the RF immunity evaluation, Silicon Labs’ isolator was free of errors even in the presence of 20 V/m RF energy.

 

In his own words, Mr. Lumio writes, “Digital isolators from Silicon Laboratories were in the top group of manufacturers in all of the tests.” His thesis is additional evidence for the suitability of CMOS isolators in demanding applications that require high reliability, like motor drives. We’re proud that Silicon Labs’ capacitive based isolation fared well in all of Mr. Lumio’s analysis and it’s our goal to deliver higher performance, more reliable isolated circuits than competing solutions. For more information, visit our Isolations Solutions page.

 

  • Blog Posts

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
  • 2021 February
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • A Guide to IoT Protocols at Works With...
  • IoT Hero Rainus Enhances the In-Store Shopping...