I need a low power standalone module that supports Bluetooth Mesh that can "wake on Bluetooth Mesh" (so all the BT nodes will wake up), Wake on motion (some kind of IMU on each node), Wake on audio, etc. I need it to operate at low power and only when needed to wake up a Raspbery Pi 3. Can the Thunderboard Sense support this? Is there a white paper? What is the lowest power that the Thunderboard Sense can just listen...
Bluetooth Mesh by the Numbers