Significant investment is pouring into data centers as the enterprise market accelerates its increased use of cloud-based computing solutions and the demand for lower latency intensifies. Wireless networks are also experiencing tremendous change as networks move from 4G/LTE to LTE-Advanced and 5G systems.

 

In a new whitepaper by James Wilson, Senior Marketing Director of Timing Products at Silicon Labs, details how data centers and wireless networks are equipping themselves to handle these enormous changes by adopting high-speed 100G Ethernet. Although a popular and cost-effective solution, the increased use of optical high-speed Ethernet is driving the need for high-performance clock and frequency control products in both wireless network and data center environments.  

The new paper details why clock and frequency products are playing a crucial role in these two technological evolutions. For example, several specific technical obstacles have arisen within data centers as they use the Ethernet to support the rapid shift of enterprise workloads to cloud infrastructure. The majority of data center traffic stays within the data center as workload processing is distributed across multiple computer nodes, posing a serious problem to data centers. To clear this hurdle, data centers are starting to optimize their network architecture to support distributed, virtualized computing by connecting every switch to each other, otherwise known as hyperscale computing.

The Ethernet is critical to making hyperscale possible as data center switches quickly move from 25G, to 50G, to 100G to expedite data transfer and network efficiency. This speedy migration is driving data center equipment manufacturers to upgrade switch and access ports to higher speeds, fueling the need for higher performance, lower jitter timing solutions. Ultra-low jitter clocks and oscillators are necessary in these applications because high clock noise can result in unacceptably high bit-error rates or lost traffic.

As the paper details, mobile networks are also experiencing seismic change as operators prepare to support mobile data traffic expected to grow by 49 exabytes per month by 2021, a sevenfold increase since 2016. To meet the aggressive bandwidth demands, wireless networks are being re-architected and optimized for data transport with widescale adoption of high-speed Ethernet in radio access networks (RAN). The whitepaper lays out how the wireless industry is starting to re-envision base station architectures. Unlike the distributed model of 4G/LTE, where RF and baseband processing functions were split into separate remote radio heads (RRH) and base band units (BBU), the connection between baseband and radio elements, known as the fronthaul network, are being optimized for LTE-Advanced/5G networks.

To ensure fronthaul networks can handle the new bandwidth constraints being placed on them with the proposed new architecture, numerous standards have developed. Highlighted in detail within the paper, the new fronthaul standards are driving the need for frequency flexible timing solutions that can support both LTE and Ethernet clocking in radio heads, small cells, and pico cells. These new solutions provide the opportunity for hardware designs to unify all clock synthesis into a single, small-form factor IC.

For wireless infrastructure and data center architects, the paper is a must read. Providing readers with detailed architecture and IC illustrations, the article will give readers better perspective on effectively leveraging the Ethernet while maintaining flexible, accurate timing and synchronization – which ultimately, prevents the loss of traffic and/or data error in either environment.

 

Read the full paper here.

 

 

 

 

 

  • Blog Posts
  • Timing