Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Timing 101 #7: The Case of the Spurious Phase Noise Part II

02/58/2018 | 12:17 AM
Lance Looper
Employee

Level 5


Hello and welcome to another chapter in our Timing 101 series from Silicon Labs' Kevin Smith.

Introduction

In this article, I want to continue last month’s discussion regarding spurs in clock phase noise measurements. There were a few items I just couldn’t include previously due to lack of time and space.

You will recall from last time that spurs are discrete frequency components in clock phase noise plots. Spurs are typically few and low amplitude, but generally undesirable as they contribute to a clock’s total jitter. 

However, spurs can also be used for evaluation and characterization of timing devices. We can use lab sources configured for low-level modulation to apply spurious frequency components, directly or indirectly, as input stimuli to a clock device or system. The resulting output clock spurs are then measured with a spectrum analyzer or phase noise analyzer.  

In this post, The Case of the Spurious Phase Noise Part II, I will briefly review suitable signal modulation options.  Next I will discuss some notable measurements.  Finally, I will give results for a select example, jitter transfer.

 

Modulation Selection, i.e. Not All Spurs are Created Equal

There are three basic analog modulation options to most lab grade generators, i.e., AM, FM, or PM, referring to Amplitude Modulation, Frequency Modulation, and Phase Modulation, respectively. Each have their place in our “spur toolbox.” But first a digression. Consider each of the spectrum analyzer screen caps below. The carrier is nominal 100 MHz and there are a pair of symmetric spurs on each side at 100 kHz offset from the carrier.  Each spur is about 60 dB down from the carrier.

Can you tell which screen cap corresponds to AM, FM, or PM? No, not really, not without additional information. In this particular example, the images are in alphabetical order.

So, why are they so hard to distinguish? There are several reasons:

  1. A spectrum analyzer measures only the amplitude of the spectra, but not the phase.  In this sense, it acts like a voltmeter.  See for example Keysight Technologies’ Spectrum Analysis Basics app note.
  2. FM and PM are both angular modulation methods that behave the same way and really only differ by their modulating function. An FM signal can produce PM and vice-versa.
  3. Finally, at low modulation indices, AM, FM and PM sideband amplitudes look very similar.

Let’s look at the last couple of points in some detail.  The following relations are adapted from the appendix in Keysight Technologies’ Spectrum Analysis Amplitude and Frequency Modulation app note.

 

Note: These FM components are the same magnitude as for AM, but unlike AM there is a minus sign in front of the lower sideband. However, since the spectrum analyzer does not preserve phase information, low modulation AM, FM, and PM components look the same.

In general, the SSB or single sideband spur to carrier ratio of AM, FM, or PM is 20*log10 (Modulation Index/2). For example, given 200 Hz peak-peak frequency deviation and 100 kHz frequency modulation, we expect a SSB spur as follows:

SL = 20 log10 {(200/2)/100E3} = -60 dBc

Now, here’s the practical aspect of using FM versus PM. If your source supports PM, then you can directly enter the amount of peak phase modulation. You need not change this setting as you step the modulation frequency or spur offset frequency.  However, if your source only supports FM, then the frequency modulation index must be maintained per the following relation.

In this case, you will need to scale the peak frequency deviation Delta-f together with the modulation frequency fm in order to keep Beta constant.

So What Tests Can We Do with Modulation Spurs?

Generally, we will measure output clock spurs in the frequency domain using either a spectrum analyzer or a phase noise analyzer. We choose different modulation methods depending on what stimulus we need to apply to the system.  The table below summarizes some notable measurements. I will briefly discuss each of these tests and then focus on the last one in a bit more detail.

You will note that either FM or PM can be used to generate input clock spurs for jitter transfer testing. The only thing you will need to keep track of is the phase or frequency modulation index. Modern AWGs (Arbitrary Waveform Generators) typically support AM, FM, and PM.  Higher frequency RF and Microwave signal generators also support at least FM.

 

Here are some more details about each of the tests mentioned in the table.

Input AM-to-PM Conversion

A high gain well designed clock buffer will tend to reject AM and only pass along phase (timing) error. However, no input clock buffer is perfect and some AM-to-PM conversion can take place. The mechanism and amount of such conversion will in general differ depending on the modulation frequency. 

The set-up for this test is straight forward, i.e. apply an input clock with AM and then check for an output clock spur offset at the amplitude modulation frequency.  There are a few considerations to keep in mind when doing this type of test:

  • Keep the modulation index low so there is practically only a single sideband spur of consequence.
  • Vary the modulation frequency over the regions of interest. 
  • Use a limiter on the input to the spectrum analyzer or phase analyzer so that we needn’t worry about AM-to-PM conversion in the instrument.
 

PSR

PSR or Power Supply Rejection is similar to the previous test in that AM is applied. However, in this case, it is not the input clock that is modulated.  Rather AM is introduced indirectly via the power supply and then spurs measured as before.  This type of measurement also goes by other names such as PSRR (Power Supply Rejection Ratio) or power supply ripple testing.

In addition to the earlier AM-to-PM considerations, there are a few others:

  • We usually want to remove all the bypass capacitors if possible. This eliminates one variable and makes it easier to inject fixed amplitude ripple, e.g. 100 mVpp, into the power rail over the frequency range of interest. It is also fairer when comparing devices.
  • AM needs to be injected into the power supply without impacting instruments or other system components.  We generally use a Bias Tee for this purpose.
  • Consistency is important for low level spur measurements, so try to keep set-ups the same when comparing devices.

 

This topic alone deserves much separate treatment.  Please see Silicon Labs app note AN491: Power Supply Rejection for Low-Jitter Clocks for further details. Where there are multiple rails, and/or removing bypass caps may be a performance issue, you can leave them in and simply do straightforward performance testing as described in Silicon Labs’ app note AN887: Si534X and Power Supply Noise.

 

Jitter Transfer

A relatively quick way to check the transfer curve of a clock PLL chip is to apply low level PM or FM spurs and step the modulation offset frequency from well below the expected loop bandwidth to well above it. Then using a phase noise analyzer, with Max Hold enabled, you will see how the applied spurs roll off. The intersection of the asymptotes of the spur amplitudes allows one to estimate the loop bandwidth.

You can kind of tell what’s going on by looking at the phase noise, but using a fixed modulation index input clock allows us to more precisely measure the transfer function. The 2 screen caps below were taken applying a phase modulated 25 MHz input clock (0.2° phase deviation) to an Si5345 jitter attenuator and measuring the phase noise continuously in Max Hold for a 100 MHz output clock.

In the first case, figure below, the DSPLL bandwidth is set 400 Hz. The plot shows that the annotated asymptotic lines intersect right around 400 Hz, as expected. The roll-off in the vicinity of the corner frequency is a little over 30 dB/dec.

 

In the second case, figure below, the DSPLL bandwidth is set to 4 kHz. This time the plot shows that the annotated asymptotic lines intersect around 4.5 kHz, which is a little wider than the nominal target. The roll-off in the vicinity of the corner frequency here looks closer to 25 dB/dec.

 

The use of the Max Hold feature allows us to make a “quick and dirty” manual measurement. However, we could make more careful measurements using averaging and storing spur amplitudes across ensembles of runs in order to accurately characterize the loop bandwidth of the DUT.

Conclusion

Well, that’s it for this month. In this post, I’ve extended our discussion on spurs in phase noise measurements to include some thoughts on using them for test purposes. I hope you have enjoyed this Timing 101 article.  

As always, if you have topic suggestions, or there are questions you would like answered, appropriate for this blog, please send them to kevin.smith@silabs.com with the words Timing 101 in the subject line.  I will give them consideration and see if I can fit them in. Thanks for reading. Keep calm and clock on.

Cheers,

Kevin

Below are the other Timing 101 articles:

Timing 101: The Case of the (Apparently) Jittery Jitter Attenuated Clock

Timing 101: The Case of the Ouroboros Clock

Timing 101: The Case of the Jitterier Divided-Down Clock

Timing 101: The Case of the Split Termination

Timing 101: The Case of the PLL’s VCO High Pass Transfer Function

Timing 101: The Case of the Spurious Phase Noise Part I

Timing 101 The Case of the Cycle-to-Cycle Jitter Rule of Thumb

Timing 101: The Case of the Discrepant Scope Measurements

Timing 101: The Case of the Half-terminated Differential Output Clock

 

 

 

  • Blog Posts
  • Timing

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
  • 2021 February
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • A Guide to IoT Protocols at Works With...
  • IoT Hero Rainus Enhances the In-Store Shopping...