Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Micrium OS USB-Device VENDOR Class and Demo

01/04/2019 | 06:58 PM
Fernando Flores
Employee

Level 3


The objective of this blog is to show you the steps necessary to use an existing Micrium OS USBD example and add a different class and demo using the EFM32GG11.

Baseline Project

Since the Gecko SDK currently ships with a ‘micriumos_usbdhidmouse’ project for the SLSTK3701A_EFM32GG11 board, we can make a copy of it and rename it ‘micriumos_usbdvendor’. The convenience of making a copy of the project is to modify it according to our needs without breaking the Gecko SDK default projects. Start by locating the ‘micriumos_usbdhidmouse’ folder in your Simplicity Studio installation. The project location is at ‘C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v2.5\app\mcu_example\SLSTK3701A_EFM32GG11’

Once you found the folder, make a copy of it and rename it ‘micriumos_usbdvendor’. Please make sure to keep the new folder at the same path location of the original. Locate the ‘SLSTK3701A_micriumos_usbdhidmouse.slsproj’  file inside your New Folder  ‘micriumos_usbdvendor\SimplicityStudio’ and rename it ‘SLSTK3701A_micriumos_usbdvendor.slsproj’ 

We will be adding our new workspace, so launch Simplicity Studio and connect the SLSTK3701A_EFM32GG11 board to the PC.

Add workspace by right-clicking anywhere inside the Project Explorer box and Select Import>MCU Project

vendor00

 

Use the Browse button to locate the ‘SLSTK3701A_micriumos_usbdvendor.slsproj’ and click Next>

File Location: `C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v2.5\app\mcu_example\SLSTK3701A_EFM32GG11\micriumos_usbdvendor\SimplicityStudio`

vendor01

 

Since you already have your board connected, it should all be auto-detected. Leave everything by default making sure that there is an SDK selected, then click Next>

vendor02

 

You can either change the name of the project or keep the default, then click Finish.

vendor03

 

Configuration Files

 We will now need to modify the project configuration files to include Micrium OS USBD Vendor class as part of our build. Start by expanding the Includes section in the Project Explorer panel, then expand the configuration folder as shown in the image below. After that, double-click on the rtos_configuration.h to open it in the editor.

vendor04

 

As soon as you try to edit the rtos_description.h, you will be presented a Warning indicating you are editing an SDK file. Click on Edit in SDK.

vendor05

Add the following #define in rtos_description.h to indicate Micrium OS that you want to use VENDOR class.

#define  RTOS_MODULE_USB_DEV_VENDOR_AVAIL

Remove the following #define in rtos_decription.h

#define  RTOS_MODULE_USB_DEV_HID_AVAIL

 

Tell Micrium OS you want to use the USBD VENDOR demo by modifying ex_description.h. Expand the Includes section in the Project Explorer panel, then expand the project folder as shown in the image below. After that, double-click on the ex_description.h to open it in the editor.

vendor06

As soon as you try to edit the ex_description.h, you will be presented a Warning indicating you are editing an SDK file. Click on Edit in SDK.

vendor07

Remove the following #define in ex_description.h

#define RTOS_MODULE_USB_DEV_HID_AVAIL

Add the following #define in ex_description.h  to indicate Micrium OS you want to use VENDOR class.

#define  RTOS_MODULE_USB_DEV_VENDOR_AVAIL

 

Adding USBD Class and Demo

Expand the src section in the Project Explorer panel and remove the ‘ex_usbd_hid_mouse.c’ linked file.

vendor08

 

Select Import > MCU Project by right-clicking on src section as shown on image below

vendor09

 

Choose ‘More Import Options…’  and select File System  on the next window that pops-up as shown on the images below

vendor10

vendor11

 

Add ‘ex_usbd_vendor_loopback.c’ example as shown on image below, and click Finish.

File location: 'C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v2.5\app\micrium_os_example\usb\device\all'

vendor12

 

Expand the usb>source>device>class section in the Project Explorer  panel and right-click on class. Select Import > MCU Project  and add the USBD VENDOR class file as shown on images below

vendor13

vendor14

vendor15

 

Use the Browse button to locate the  VENDOR class files to be added as shown below.

File location:  'C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v2.5\platform\micrium_os\usb\source\device\class'

vendor16

 

Running the Example

You can now build your application and flash it on the board. Once the application starts running, you should see LED0 on the board blinking which means all the initialization was done correctly; therefore, we can now test the USBD VENDOR demo.

Use a Micro-USB B cable to connect the PC to the EFM32GG11 board. As soon as you connect it, Windows will enumerate the device and display it in 'Universal Serial Bus Devices' as shown in the image below. 

vendor17

Execute the Windows USB application provided in the attachment (Located at 'App\Host\OS\Windows\Vendor\Visual Studio 2010\exe\x86') and provide the number of transfers.

vendor19

 

  • Blog Posts
  • Micrium OS
  • Giant Gecko S1
  • 32-bit MCUs
  • 32-bit MCU SDK
  • Microcontrollers
Windows-App.zip

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
  • 2021 February
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • A Guide to IoT Protocols at Works With...
  • IoT Hero Rainus Enhances the In-Store Shopping...