Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Timing 201 #6: The Case of the Autonomously Resetting Clock Generator

06/161/2020 | 08:34 PM
kgsmith
Employee

Level 5


Introduction

Some five years ago, a customer contacted us thinking they needed to return a clock generator device that would often go into a continuously resetting state after power-up.  We had never heard of such unusual behavior and wondered if there was anything wrong with this particular unit’s POR (Power On Reset) circuit. 

Fortunately, the customer had a small PC board that frequently exhibited the behavior, and which they could ship to us for troubleshooting in our lab.  This enabled us to more quickly determine the root cause and verify the solution.

It turned out that an overlooked spec for a passive component located elsewhere on the board was causing large consequences for the customer’s application. The lessons learned are generally applicable and the subject of this blog article, The Case of the Autonomously Resetting Clock Generator.

 

BLUF (Bottom Line Up Front)

The clock generator’s POR circuit was not at fault. In fact, it was behaving exactly as it should. Rather, an external 3.3 V regulator circuit was marginally stable. Oscillations on the 3.3 V rail could be sufficiently large to trigger autonomous resets.    

 

Browsing the Power Supply Voltages

The customer board took in +12 V and regulated this down to the +3.3 V and +1.8 V rails required by the Si5341 clock generator.  I used a lab power supply with pushbutton Output On/Off to provide the necessary +12 V input. This allowed me to manually and conveniently power cycle many times in order to observe and contrast a passing versus failing (continuously resetting) power-up event. The series of oscilloscope screen captures below display the 3.3 V (orange trace) at the top and the 1.8 V (blue trace) at the bottom.

The figure below shows the nominally settled behavior of the 3.3 V and 1.8 V after a failed power-up.  The 1.8 V supply is completely accurate. However, the 3.3 V supply is clearly oscillating and even periodically dropping down to about 2.4 V, far below the POR trip threshold. 

What about those occasions where the part successfully powers up? Per the figure below, both the 3.3 V and 1.8 V rails are at their nominal targets but the 3.3 V supply appears much noisier. This is another clue that the 3.3 V regulator circuit may be marginally stable.

I then looked at the start-up behavior. When the device fails, the 3.3 V supply starts oscillating straight away.

Even when the unit successfully powers up, as depicted below, the 3.3 V supply exhibits overshoot before settling down to a noisy nominal voltage.

 

An Informative Vendor Data Sheet

The customer was using a 500 mA LDO (Low Drop Out) regulator in a SOT-23-5 package. Reading the vendor’s data sheet, I noticed that the typical application drawing showed the output capacitor as a 2.2 uF tantalum.  Further, the data sheet explicitly stated that the output capacitor needed an ESR of about 1 Ω and that ultra-low ESR caps could cause oscillation.

Inspecting the output cap on the customer’s board revealed that it was a ceramic capacitor. These can have an ESR with an order of magnitude less than an electrolytic capacitor. So that suggested the next experiment to try.

 

Demonstrating the Fix

We hacked in a 1 Ω resistor in series with the ceramic capacitor in order to emulate the approximate ESR of a tantalum capacitor. A close-up photo of the hack is shown below. The brown component in the upper part of the “elbow” is the existing capacitor. The component marked “01Y” is the 1 Ω resistor.  

The hack was ugly but effective:

As the resulting screen cap shows above, the 3.3 V supply is much less noisy and the start-up transient is very small and quickly damped out. After many attempts, no autonomous resets were observed, current draw was as expected, and the device always yielded output clocks.  This outcome was good enough for the customer to take over and do additional verification testing for their particular application.

 

Some Lessons Learned

This Timing 201 case exemplifies several lessons learned. These are listed below, going from the general to the specific.

  1. If you have a significantly puzzling problem, and can ship us a failing PC board, that can greatly speed up the overall debug process. I realize that may not always be possible due to availability, expense, intellectual property, or power/control issues. Reducing a failing board down to the lowest populated version may help mitigate some of these concerns.
  2. When troubleshooting any functional device issue, it’s always worth double-checking the supply voltages. Regulator instabilities, more subtle than this case, may even show up as increased output clock phase noise or spurs.
  3. Be aware that relatively older LDO regulators may have been designed for and require higher ESR caps than relatively newer LDO regulators.  The particular vendor used by this customer sells LDO regulators of both varieties, i.e. those that require 1 Ω ESR output stability caps and those that do not.
  4. Finally, it’s a good idea to make sure that schematics and BOMs call out exactly what LDO output capacitor is needed so that no one accidentally orders and installs the wrong type.

 

Conclusion

I hope you have enjoyed this Timing 201 article.  

As always, if you have topic suggestions, or there are questions you would like answered, appropriate for this blog, please send them to kevin.smith@silabs.com with the words Timing 201 in the subject line. I will give them consideration and see if I can fit them in. Thanks for reading. Keep calm and clock on.

Cheers,
Kevin

  • General Purpose Jitter Attenuators
  • Blog Posts
  • General Purpose Clock Generators
  • Clock Generators
  • timing

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • IoT Hero CoreTigo Drives New Wireless Standard...
  • A Guide to IoT Protocols at Works With...