Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Five Powerful Bluetooth Dev Kit Features for Rapid IoT Prototyping

01/12/2021 | 08:08 AM
tmonte
Employee

Level 7


As a developer, you know that not all dev kits are equal. The features can make a huge difference in your development process. While most development kits out there do their job just fine – i.e., allow you to convert an idea into a prototype with a decent effort, there are also poorly designed kits, which can turn your project into a nightmare. However, an excellent development kit removes many headaches from your work, speeds up tracing and debugging, and provides interfaces for expansion.

But what makes a great Bluetooth dev kit? In this blog, we look at five powerful features that can accelerate IoT prototyping and enable you to create epic IoT products rapidly! 

 

What's Rapid IoT Prototyping?

Rapid IoT prototyping sounds like yet another buzzword brewed inside the developer community. However, it's more than that. Rapid prototyping perfectly captures the way IoT products are created today. Developers build multiple iterations of their software and hardware design quickly and get early user feedback. This allows them to adjust the design based on actual user-experience and finalize a successful prototype rapidly.

There are two types of development tools for rapid IoT prototyping. You can build a prototype on Arduino or Raspberry Pi and complete the project with another, more professional software and hardware platform. However, more advanced developers prefer to craft everything from scratch with dev kits based on commercial chipsets – they allow more room for customization, and the final build is closer to a real product rather than a hobbyist experiment.

So, what do you need from a dev kit to rapidly prototype an epic Bluetooth IoT product? Here's a rundown of five powerful Bluetooth dev kit features that speed up your development work:

 

1. Built-in Debugger   

You spend a significant share of your prototyping time debugging software and hardware. A debugger is perhaps the most critical component of a Bluetooth dev kit, yet many available kits do not come with a debugger!

When choosing your next Bluetooth dev kit, make sure it hosts an on-board debugger to avoid having to buy a separate board. A debugger built on the board streamlines your dev work because you can simply flash the code and debug as it runs in the target processor. Also, on-board debuggers are typically compatible with the vendor's integrated development environment (IDE), giving you more advanced debugging capabilities.

All in all, a Bluetooth Dev Kit with a built-in debugger saves you from buying an extra board, minimizes the hassle, and speeds up development work and prototyping.

2. Bluetooth Traffic Tracer

Developing wireless products, including Bluetooth devices without a traffic tracer, is hard. You can't see what's going on in the wireless link when you run into issues in the Bluetooth protocol level without a tracer, which makes troubleshooting pure guesswork.

A dev kit with a built-in packet tracing interface, on the other hand, allows you to capture the raw Bluetooth traffic flowing into the system and analyze it with a network analyzer tool. The analyzer decodes the data into a human-readable BLE protocol format, which makes debugging a breeze.

A packet tracer interface on a Bluetooth dev kit offers invaluable debug information about transmitted and received packets in wireless links, removes the guesswork from debugging, and speeds up prototyping significantly.

3. Virtual Com Port

When kicking off prototyping, the first thing you do is to set up a serial line between the target and PC to get data logging going and commands flowing back to the processor. This allows high-level debugging – you can find out which parts of the code are not working before making the first deep-dive.

Getting a Bluetooth dev kit with a built-in virtual com port will save you from buying an external board for UART-to-USB bridging, and, again, you can remove much hassle from your project and get your prototype off the dev board faster.

4. Generic BLE Mobile App Tester with OTA

Let's face it; nobody wants to buy a Bluetooth IoT product in 2021 without a smooth smartphone App and over-the-air (OTA) software update. Suppose you want to develop excellent smartphone connectivity and OTA capability for your product, a Bluetooth dev kit with support for a generic BLE mobile app tester with OTA should be on your shopping list. It will save significant development time and helps you to launch a convincing, market-ready prototype rapidly.

5. Hardware Ecosystem Support

No developer wants to waste precious time building every component from scratch, especially when many hardware ecosystems offer vast amounts of off-the-shelf components. However, with a dev kit, which lacks standard interfaces to hardware ecosystems, you can forget about rapid prototyping – you are doomed to spend ages creating everything ground-up by yourself or wiring up dodgy, no-name components without proper documentation.

A Bluetooth dev kit equipped with the MikroBUS™ socket allows you to instantly expand your project with hundreds of auxiliary hardware components, including Click boards developed by MikroE.

However, if you don't' find what you need from MikroE's portfolio, you have other options such as the Qwiic® Connect System from Sparkfun, which is compatible with a range of boards provided by Sparkfun, as well as Adafruit, and Seeed Studio. Via the Qwiic interface, you can chain up add-on boards over the I2C interface and build up your dev kit with more functionalities (e.g., sensors, LCDs, and other peripherals) as if they were Lego bricks.

 

The IoT revolution is like one big innovation contest – developers worldwide turn their wildest ideas into products. Only the fastest developers can win, and that's why rapid prototyping has become the most popular market entry strategy in IoT. As a developer, you want to get a head-start in this race and buy the dev kit with the best bang for your buck – such as Silicon Labs Explorer Kit, which provides you all the five power-features, and more, as the only Bluetooth Dev Kit in the $10 price range!

  • Blog Posts
  • Bluetooth SDK

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • IoT Hero CoreTigo Drives New Wireless Standard...
  • A Guide to IoT Protocols at Works With...