Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Official Blog of Silicon Labs

  • Show More
    Publish
    • Immediately
    • Draft
    • At scheduled date and time
     
      • IoT Hero Boundary Delivers Simplified, User-Friendly Home Security for DIY Homeowners

        Jackie Padgett | 12/353/2020 | 03:26 PM

        Home security device manufacturers in the UK are required to adhere to a complicated set of British and European standards before their products can hit the market, which typically requires professional installation. A consequence of this relatively high barrier to entry is that most of the available alarm solutions are professional grade and, due to these regulations, must be segregated from other smart home assistance. Scotland-based Boundary is working on bridging this gap with a state-of-the-art alarm system that consumers can install themselves and monitor through their smartphones. We recently sat down with Boundary co-founder, Paul Walton to learn more.

        Boundary and Silicon Labs Smart Home

        Tell Us About Boundary.

        Boundary was founded in 2018 after a successful Kickstarter campaign, producing a smart intruder alarm system for the UK market based on Z-Wave technology. Our co-founder, Robin Knox, had the idea when he was on his honeymoon and realized the limitations of his existing alarm system meant that if his home was broken into, he would be unable to actually do anything other than watch the events unfold on a CCTV camera. Immediately upon his return, he set out to find a reasonably priced self-install security system but had little success. This gap in the market for DIY home security was the catalyst to build something that looked great, was user-friendly, and provided better features at a reasonable price point.

        Internally, our company’s goal was to develop a great mobile app that provided a much more intuitive and enjoyable user experience. With a focus on the user journey and hardware design, we are anticipating launching our first product, a smart IoT alarm system, this month. This system consists of four components: the central hub (which is the Z-Wave gateway), a motion sensor, a contact sensor, and an external siren, all of which connect to the central hub advisory.

        One thing that sets Boundary apart from our competitors is its EN50131 European Standard for Intruder Alarm Systems compliance certification. Achieving this level of certification requires some pretty tough validation, dropping the hub from two meters and making sure that it's still operational, for instance. The rigorous design detail has made us the first manufacturer of a Z-Wave 700 device that is currently undergoing this certification, which is expected to be completed in the first quarter of next year.

        Why Did You Choose Silicon Labs Z-Wave Solutions for Your Products?

        When it came to selection criteria, we had many requirements that needed to be met. Some were driven by the standards and some were simply a matter of the target data transmission rates the team wanted to meet. Developing a product that did not require complicated setup and provided the range required to cover a medium-to-large sized house was also important, as was maintaining connection for all devices on the network. Z-Wave emerged as the standard that could meet these challenges. Set-up is incredibly simple, requiring the customer to simply scan a QR code to pair the device.  

        The result is an alarm that is easy to use and exceeds the highest regulatory standards. Our product features a motion sensor with always-on detection that can be used for home automation routines like powering down smart lighting and regulating heating when a room is not in use. With a door/window sensor, any unauthorized entry will immediately set off the alarm. Users can also see the status of a window or door from the app at any time.

        Looking Forward, Where Do You See the Smart Home Security Market Heading?

        We believe that within the next five years, we’ll see a bit of a shift in the home security market towards proactive security. For Boundary, our focus is on bringing another product to market, one that utilizes machine vision, and to expand into Europe.

        For more information on how Boundary used Silicon Labs Z-Wave solutions to deliver professional-grade security to smart homes, check out our case study and learn more about smart home offerings.  If you’d like to leverage the benefits of Z-Wave technology for your smart home applications, we’d love to hear from you. 

      • Timing 201 #8: The Case of the Dueling PLLs – Part 2

        kgsmith | 12/351/2020 | 09:52 PM

        Introduction

        In the previous Timing 201 article, Timing 201 #7: The Case of the Dueling PLLs – Part 1, I referred to a Silicon Labs white paper that describes Silicon Labs’ DSPLL nested dual-loop architecture as used in the Si538x wireless jitter attenuators. I first discussed the general motivation for a dual-loop PLL and compared the cascaded (series) dual-loop PLL versus the nested dual-loop PLL architectures.

        The practical advantages of the nested dual-loop approach in this example were to reduce the number of tuned oscillators from 2 to 1 and to eliminate the need for a sensitive external voltage control line. The tradeoff for a nested feedback control loop is that the inner loop must be faster than the outer loop. If the loop speeds (or bandwidths) are comparable, then the loops will contend or “duel” with each other.

        In this Part 2 follow-up post, I will discuss in more detail how to calculate the phase noise of both these dual-loop PLL approaches.


        Some Simplifying Assumptions

        To emphasize the basic ideas without getting bogged down in too much detail, I will make the following simplifying assumptions:

        1. Jitter generation, i.e., intrinsic PLL noise, is negligible. I only care about how the PLLs filter their respective phase noise sources, and how they contribute to the output clock phase noise.
        2. Phase noise scaling is not needed. Assume that the phase noise data I use is taken at the same carrier frequency for both PLLs. For example, it’s as if you had a 54 MHz XO or VCXO, and the input and output clock frequencies were all 54 MHz, and the VCO phase noise had been scaled down to 54 MHz. (Otherwise you would need to scale the phase noise data.)
        3. Identical phase noise sources will be used to compare the two topologies. In particular, the XO and VCXO phase noise will be assumed to be identical. This is generally not the case as VCXOs are usually noisier than XOs for the same nominal frequency. Why this assumption is being taken will be made clear later in this article.
        4. The PLL acts as a low pass filter (LPF) or high pass filter (HPF) to the input and VCO phase noise respectively. The filter is modeled with the corner frequency at the bandwidth (BW) frequency. The filter skirt slope or steepness magnitude is 20 dB/dec x the PLL order. So, a 2nd order PLL will be modeled with 40 dB/dec filter slopes.    


        Series Dual-Loop Phase Noise Calculations

        The figure below is from the cited white paper and previous post. The two PLLs are in series with each other.  

        You will recall that the first PLL, PLL1, is narrowband (NB) and the second PLL, PLL2, is wideband. To calculate the phase noise, we will go left to right through the following steps.

        1. Low pass filter the input clock phase noise based on PLL1’s bandwidth (BW).
        2. High pass filter the VCXO phase noise based on PLL1’s BW.
        3. Add their contributions together in a power sense to yield the total PLL1 phase noise input to PLL2.
        4. Low pass filter the input to PLL2 based on PLL2’s BW.
        5. High pass filter the VCO phase noise based on PLL2’s BW.
        6. Finally, add these last two contributions together in a power sense to yield the total output phase noise

        These calculations have been done in the attached spreadsheet Timing_201_7_The_Case_of_the_Dueling_PLLs - Part 2.xlsx. See the “Series Dual-Loop” worksheet. The PLLs are assumed to be 2nd order with the NB PLL BW = 100 Hz and the WB PLL BW = 1 MHz. These parameters can be changed in the spreadsheet, but practically speaking, NB PLLs will be on the order of mHz to kHz. WB PLLs are typically 500 kHz to 2 MHz. 

        The resulting plot is as follows.

         

        Nested Dual-Loop Phase Noise Calculations

        The figure below is also repeated from the cited white paper and previous post. In this case, the two PLLs are nested with respect to each other. 

        Now the inner loop (IL) PLL is WB and the outer loop (OL) PLL is NB. To calculate the phase noise, we will proceed from the “inside out” through the following steps.

        1. Low pass filter the XO phase noise based on the IL PLL’s BW.
        2. High pass filter the VCO phase noise based on the IL PLL’s BW.
        3. Add their contributions together in a power sense to yield the total IL phase noise. Recall that the IL PLL acts as the “VCO” of the OL PLL.
        4. Low pass filter the input phase noise based on the OL PLL’s BW.
        5. High pass filter the total IL phase noise based on the OL PLL’s BW.
        6. Add these last two contributions together in a power sense to yield the total output phase noise. 

        These calculations have also been done in the attached spreadsheet Timing_201_7_The_Case_of_the_Dueling_PLLs - Part 2.xlsx. As before, to keep things “apples to apples”, the PLLs are assumed to be 2nd order with the NB PLL BW = 100 Hz and the WB PLL BW = 1 MHz.  See the “Nested Dual-Loop” worksheet. The resulting plot is as follows.

        You will note how similar these plots are to each other. Let’s overlay the output phase noise plots together for comparison.
         

        Series versus Nested Dual-Loop Phase Noise Plots

        The output phase noise plots are overlaid on top of each other for direct comparison. As shown, they look identical. Further, if you experiment with the bandwidths of each PLL, for each topology, the best output phase noise is generally obtained by making PLL1 (or OL PLL) and PLL2 (or IL PLL) narrowband and wideband respectively. Even apart from stability considerations, both topologies benefit from wide separation between the bandwidths.  

         

        Why the Topological Equivalence?

        This result is not necessarily to be expected so let’s walk through the steps again and compare the approaches.

        1. The total series dual-loop phase noise can be written out as:

        LPF_WB (LPF_NB (Input) + HPF_NB (VCXO)) + HPF_WB (VCO)
        LPF_WB * LPF_NB (Input) + LPF_WB * HPF_NB (VCXO) + HPF_WB (VCO)

        The use of WB and NB notation versus PLL1, PLL2, IL PLL, and OL PLL is to help us make direct comparison between the two sets of calculations. LPF_WB means apply a wideband low pass filter to the phase noise in parenthesis. Two filter terms multiplied indicates applying both filters. 

        1. Similarly, the total nested dual-loop phase noise can be written out as:

        LPF_NB (Input) + HPF_NB (LPF_WB (XO) + HPF_WB (VCO))
        LPF_NB (Input) + HPF_NB * LPF_WB (XO) + HPF_NB * HPF_WB (VCO)

        1. If the bandwidths involved are the same, and the VCXO phase noise equals the XO phase noise, then the center terms above are equivalent. These can be thought of as the “bandpass” terms.
           
        2. Further, assuming sufficient separation between bandwidths, we can make the following approximations:

        LPF_WB * LPF_NB (Input) ≈ LPF_NB (Input)
        HPF_NB * HPF_WB (VCO) ≈ HPF_WB (VCO)

        In other words, the NB LPF and the WB HPF dominate the calculations for these LPF and HPF terms. This is why these topologies produce equivalent total phase noise when all else is equal.
         

        Conclusion

        I hope you have enjoyed this Timing 201 article. In this Part 2 follow-up post, I have discussed in more detail how to calculate the phase noise of both the series and nested dual-loop approaches. Finally, by using a simplified example with widely separated bandwidths, we can see that the approaches are essentially equivalent. There are particular advantages to the nested dual-loop approach which arise from an alternate practical implementation that yields phase noise equivalent to the series dual-loop approach.  

        As always, if you have topic suggestions or questions appropriate for this blog, please send them to kevin.smith@silabs.com with the words Timing 201 in the subject line. I will give them consideration and see if I can fit them in. Thanks for reading. Keep calm and clock on.

        Cheers,
        Kevin

        Timing_201_8_The_Case_of_the_Dueling_PLLs - Part 2.xlsx

      Tags

      • Wireless
      • High Performance Jitter Attenuators
      • EFR32FG22 Series 2 SoCs
      • EFR32MG21 Series 2 SoCs
      • Security
      • Bluegiga Legacy Modules
      • Zigbee SDK
      • ZigBee and Thread
      • EFR32BG13 Series 1 Modules
      • Internet Infrastructure
      • Sensors
      • Wireless Xpress BGX13
      • Blue Gecko Bluetooth Low Energy SoCs
      • Z-Wave
      • Micrium OS
      • Blog Posts
      • Low Jitter Clock Generators
      • Bluetooth Classic
      • Makers
      • Flex SDK
      • Tips and Tricks
      • timing
      • Smart Cities
      • Smart Homes
      • IoT Heroes
      • Reviews
      • RAIL
      • Simplicity Studio
      • Tiny Gecko
      • EFR32MG22 Series 2 SoCs
      • Mighty Gecko SoCs
      • Timing
      • Temperature Sensors
      • Blue Gecko Bluetooth Low Energy Modules
      • Ultra Low Jitter Clock Generators
      • General Purpose Clock Generators
      • EFR32BG22 Series 2 SoCs
      • Industry 4.0
      • Giant Gecko
      • 32-bit MCUs
      • Bluetooth Low Energy
      • 32-bit MCU SDK
      • Gecko
      • Microcontrollers
      • Jitter Attenuators
      • EFR32BG21 Series 2 SoCs
      • News and Events
      • Wi-Fi
      • Bluetooth SDK
      • Community Spotlight
      • Clock Generators
      • Biometric Sensors
      • General Purpose Jitter Attenuators
      • Giant Gecko S1
      • WF200
      • Flex Gecko
      • Internet of Things
      • 8-bit MCUs
      • Oscillators
      • Wireless Jitter Attenuators
      • Isolation
      • Powered Devices
      • Power

      Top Authors

      • Avatar image Siliconlabs
      • Avatar image Jackie Padgett
      • Avatar image Nari Shin
      • Avatar image lynchtron
      • Avatar image deirdrewalsh
      • Avatar image Lance Looper
      • Avatar image lethawicker

      Archives

      • 2016 April
      • 2016 May
      • 2016 June
      • 2016 July
      • 2016 August
      • 2016 September
      • 2016 October
      • 2016 November
      • 2016 December
      • 2017 January
      • 2017 February
      • 2017 March
      • 2017 April
      • 2017 May
      • 2017 June
      • 2017 July
      • 2017 August
      • 2017 September
      • 2017 October
      • 2017 November
      • 2017 December
      • 2018 January
      • 2018 February
      • 2018 March
      • 2018 April
      • 2018 May
      • 2018 June
      • 2018 July
      • 2018 August
      • 2018 September
      • 2018 October
      • 2018 November
      • 2018 December
      • 2019 January
      • 2019 February
      • 2019 March
      • 2019 April
      • 2019 May
      • 2019 June
      • 2019 July
      • 2019 August
      • 2019 September
      • 2019 October
      • 2019 November
      • 2019 December
      • 2020 January
      • 2020 February
      • 2020 March
      • 2020 April
      • 2020 May
      • 2020 June
      • 2020 July
      • 2020 August
      • 2020 September
      • 2020 October
      • 2020 November
      • 2020 December
      • 2021 January
      • 2021 February
      • 2021 March
      • 2021 April
      Silicon Labs
      Stay Connected With Us
      Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
      • About Us
      • Careers
      • Community
      • Contact Us
      • Corporate Responsibility
      • Privacy and Terms
      • Press Room
      • Investor Relations
      • Site Feedback
      • Cookies
      Copyright © Silicon Laboratories. All rights reserved.
      粤ICP备15107361号
      Also of Interest:
      • Bring Your IoT Designs to Life with Smart,...
      • Using Wi-Fi for Low Power IoT Applications
      • A Guide to IoT Protocols at Works With...