Silicon Labs Silicon Labs Community
silabs.com
Language
  • 简体中文
  • 日本語
  • MCUs
    • 8-bit MCU
    • 32-bit MCU
  • Wireless
    • Bluetooth
    • Proprietary
    • Wi-Fi
    • Zigbee & Thread
    • Z-Wave
  • More Products
    • Interface
    • Isolation
    • Power
    • Sensors
    • Timing
  • Development Tools
    • Simplicity Studio
    • Third Party Tools
    • Thunderboard
  • Expert's Corner
    • Announcements
    • Blog
    • General Interest
    • Projects
  1. Community - Silicon Labs
  2. Blog

Official Blog of Silicon Labs

  • Show More
    Publish
    • Immediately
    • Draft
    • At scheduled date and time
     
      • Simplify Low-Power, Cloud-Connected Development

        Lance Looper | 02/54/2018 | 01:24 PM

        For the upcoming Embedded World tradeshow in Nuremberg, Germany, the Silicon Labs MCU team is showing off some unique ways to ease the challenges of developing cloud-connected applications. The demo consists of the EFM32 Giant Gecko 11 MCU, which is running Micrium OS and connects to Amazon Web Services via the new XBee3 cellular module from Digi International.

         

        This particular demo is quite simple – a closed-loop system with an MCU monitoring a temp sensor and controlling a fan. However, the real-world use cases that these building blocks and tools can scale to serve are much more profound.

        For example, many smart city applications including bridge sensors, parking meters, waste management sensors, and others often consist of portable sensor devices that require seamless long-range connectivity to the cloud. They may be battery powered with user demands of 10+ year battery life. They may have lots of sensor inputs and extra features like button inputs and local displays. Finally, they might need to be designed quickly, but with a long field-upgradeable lifetime in mind. These are the types of applications that this demo speaks to, with Micrium OS, Giant Gecko 11, and Digi’s XBee3.

        Micrium OS is running on the MCU and helps modularize the application functions. It’s helping the MCU maintain communication with the cellular module, monitor the temp sensor, drive the TFT display, and update control settings when local push buttons are pressed. By using Micrium, these various pieces can easily be divided and coded in parallel without having to worry about any messy integration at the end. In fact, this is exactly what the Embedded World demo team did – three different development teams in three different cities built the demo, and Micrium was the underlying glue that made it seamlessly come together.

        Another challenge being addressed here is the connectivity piece. As devices are now adding wireless connectivity, there are lots of hurdles to clear: RF design in some cases, FCC certifications, understanding wireless networking, security, and more. Not only does Silicon Labs offer homegrown, low power SoCs and modules, but now Digi helps add simple cellular connectivity. The Digi XBee3 is a plug-and-play NB-IoT module that has built-in security and is pin-compatible with 3G and LTE-M modules. It’s programmable via MicroPython and comes pre-certified so developers can focus more on the application itself.

        This brings us to the developer’s main focus, the application. The Giant Gecko 11 is a new 32-bit energy friendly microcontroller from Silicon Labs, and our the most capable yet. It helps simplify complex, cloud-connected applications with its large on-chip memory (2MB/512kB), lots of flexible sensor interfaces, SW and pin compatibility with other EFM32 MCUs, and unique low power capability to help prolong battery life. For example, not only does Giant Gecko 11 allow for autonomous analog and sensing in “Stop Mode” (1.6 uA), but it also has Octal SPI interface for external data logging, which could be used to reduce cellular transmission duty cycling.

        There is one more unique offering in this demo. Considering that cellular connectivity might not be the solution for all IoT applications, the SW compatibility of Giant Gecko 11 and all EFM32s with Silicon Labs Wireless Geckos makes it easy to migrate to another wireless SoC or module, if needed. For example, some use cases and markets may use NB-IoT (such as this demo), while others might need their own proprietary sub-GHz solution (Flex Gecko).

        For more information about what we’re doing at Embedded World, click here: https://www.silabs.com/products/wireless/internet-of-things.

      Tags

      • Wireless
      • High Performance Jitter Attenuators
      • EFR32MG21 Series 2 SoCs
      • Blue Gecko Series 2
      • Zigbee SDK
      • ZigBee and Thread
      • Internet Infrastructure
      • Sensors
      • Blue Gecko Bluetooth Low Energy SoCs
      • Z-Wave
      • Micrium OS
      • Blog Posts
      • Low Jitter Clock Generators
      • Bluetooth Classic
      • Makers
      • Flex SDK
      • Tips and Tricks
      • Smart Homes
      • IoT Heroes
      • Reviews
      • RAIL
      • Simplicity Studio
      • Mighty Gecko SoCs
      • Timing
      • Blue Gecko Bluetooth Low Energy Modules
      • Clocks
      • Ultra Low Jitter Clock Generators
      • General Purpose Clock Generators
      • Industry 4.0
      • Giant Gecko
      • 32-bit MCUs
      • blue-gecko-xpress-modules
      • Bluetooth Low Energy
      • 32-bit MCU SDK
      • Gecko
      • Microcontrollers
      • News and Events
      • Industrial Automation
      • Wi-Fi
      • Bluetooth SDK
      • Community Spotlight
      • Biometric Sensors
      • General Purpose Jitter Attenuators
      • Giant Gecko S1
      • Flex Gecko
      • Internet of Things
      • 8-bit MCUs
      • Isolation
      • Powered Devices

      Top Authors

      • Avatar image Mark Mulrooney
      • Avatar image Siliconlabs
      • Avatar image Nari Shin
      • Avatar image lynchtron
      • Avatar image deirdrewalsh
      • Avatar image Lance Looper
      • Avatar image lethawicker

      Archives

      • 2014 December
      • 2015 January
      • 2015 February
      • 2015 March
      • 2015 April
      • 2015 May
      • 2015 June
      • 2015 July
      • 2015 August
      • 2015 September
      • 2015 October
      • 2015 November
      • 2015 December
      • 2016 January
      • 2016 February
      • 2016 March
      • 2016 April
      • 2016 May
      • 2016 June
      • 2016 July
      • 2016 August
      • 2016 September
      • 2016 October
      • 2016 November
      • 2016 December
      • 2017 January
      • 2017 February
      • 2017 March
      • 2017 April
      • 2017 May
      • 2017 June
      • 2017 July
      • 2017 August
      • 2017 September
      • 2017 October
      • 2017 November
      • 2017 December
      • 2018 January
      • 2018 February
      • 2018 March
      • 2018 April
      • 2018 May
      • 2018 June
      • 2018 July
      • 2018 August
      • 2018 September
      • 2018 October
      • 2018 November
      • 2018 December
      • 2019 January
      • 2019 February
      • 2019 March
      • 2019 April
      • 2019 May
      • 2019 June
      • 2019 July
      • 2019 August
      • 2019 September
      • 2019 October
      • 2019 November
      Silicon Labs
      • About Us
      • In the News
      • Email Newsletter
      • Cookies
      • Contact Us
      • Community
      • Site Feedback
      • Investor Relations
      • Blog
      • Privacy and Terms
      • Corporate Citizenship
      Copyright © Silicon Laboratories. All rights reserved.
      粤ICP备15107361号-1