Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Official Blog of Silicon Labs

  • Show More
    Publish
    • Immediately
    • Draft
    • At scheduled date and time
     
      • Timing 201 #7: The Case of the Dueling PLLs – Part 1

        kgsmith | 11/324/2020 | 12:33 AM

        Introduction

        RF and microwave frequency synthesizers often employ multiple connected PLLs. These architectures trade off complexity in favor of improved phase noise, smaller frequency step size, and faster switching [1]. In timing applications we may also employ multiple PLLs to combine timing functions and/or shape phase noise.   

        For example, the white paper, “Optimizing Clock Synthesis in Small Cells and Heterogeneous Networks”, describes Silicon Labs’ DSPLL dual-loop architecture as used in the Si538x wireless jitter attenuators intended for small cell applications [2].  This particular approach is a nested dual-loop as opposed to a cascaded (concatenated) dual-loop. There are definite advantages to this implementation and some important considerations.

        One consideration is the necessary bandwidth relationship between the inner and outer loops. This topic leads to the play on words in the main title of this blog post, The Case of the Dueling PLLs.  A second consideration is the difference in how one analyzes the phase noise for such an architecture, which arises from the fundamental difference between these two approaches as explained below. 

        General Motivation for a Dual-Loop PLL Architecture

        As you may recall from a previous blog post, there are two basic PLL clock applications [3]:

        • Clock Generator (aka clock multiplier, frequency multiplier, etc.)
        • Jitter Attenuator (aka jitter cleaner)

        Low noise references are input to clock generators, which are usually wide bandwidth (e.g., 100s kHz to MHz). By contrast, jittery clocks are input to jitter attenuators, which are usually narrow bandwidth on the order of kHz or less.

        But what if your clock application requires both functions? The most straightforward approach is to cascade the two PLLs in series as discussed in the next section. 

        Cascaded Dual-Loop PLL Architecture

        The figure below, taken from the cited white paper, illustrates a single-chip, cascaded dual-loop architecture. (Note that this sense of the term cascade is different from classic control system terminology. Here we mean two PLLs concatenated or in series.)

        In this case, the left hand PLL1 with an analog Voltage Controlled Xtal Oscillator (VCXO) is used as a narrow band jitter attenuator stage.  The jitter attenuated clock signal is then input to the right hand PLL2, which is used as a wide band clock generator stage. The VCXO need not be very high in frequency but should have good close-in phase noise. This generally means a high Q crystal, which is why this component is typically external to the IC. This necessitates an external control voltage signal to the VCXO.

        The on-chip VCO needs to be high enough in frequency so that the divided down clock can yield the necessary output clock frequencies. It also should have low phase noise at high offset frequencies.

        This particular example is depicted as all analog with several external filter components and sensitive traces. However, there is no intrinsic reason why a cascaded dual-loop architecture could not be implemented more digitally and with filtering on-chip.

        Because the PLLs in the example above are in-series and independent, the total output phase noise can be calculated as a cascade of phase noise processing elements as described in [3].  

        Nested Dual-Loop PLL Architecture

        The figure below, also from the cited white paper, illustrates a nested dual-loop architecture. In classic control system terminology, this would actually be considered a variation of a cascade control system. For clarity, I will use the term nested here. Think of it as the PLL equivalent of nested Matryoshka dolls.

        In this case, the inner loop (IL) PLL is being used as the “VCO” or rather the Digitally Controlled Oscillator (DCO) of the outer loop (OL) PLL. This is the fundamental difference between these two approaches, which will determine how one calculates the total phase noise.

        How does this work?

        1. The output of the OL digital loop filter modulates the return path of the IL.
        2. The output of the IL VCO is in fact the fOUT in the diagram. In practice, this output frequency is divided further to yield the necessary output clocks.

        What are the advantages to this approach?

        In this particular pair of examples, we reduce the number of tuned oscillators from two (VCXO and VCO) down to one (XO and VCO). This eliminates the need for one of the loop filters (be it internal or external) and a sensitive voltage control line, which must otherwise be routed externally. This decrease in components makes for a more compact solution which reduces the overall PCB footprint.

        Could you implement a nested dual-loop with a VCXO?

        Yes, in principle. There is no intrinsic reason why you couldn’t implement a nested dual-loop architecture that also uses an external VCXO.  Such an approach might even make sense if a particular VCXO has better phase noise performance, perhaps at a higher frequency (update rate). However, you would lose the specific advantages discussed previously. This is why the Si538x wireless jitter attenuators do not support an external VCXO.

        What exactly is the Duel?

        In these types of nested feedback control loops, the inner loop must be faster than the outer loop. If the loop speeds are comparable, then the loops will contend or “duel” with each other.

        In PLL terms the inner loop must have a wider bandwidth than the outer loop.  This should make intuitive sense if you consider the relative difference in impact of inserting a really slow “DCO” into an otherwise fast PLL versus inserting a really fast “DCO” into an otherwise slow PLL. The former case significantly impacts the PLL and may even have stability or locking issues due to inserted additional delay. By contrast, the latter case is not impacted significantly. This tells us that the inner loop must be the faster (wider bandwidth) clock multiplier and the outer loop must be the slower (narrow bandwidth) jitter attenuator. Further, it tells us that at start-up and during the lock process, we want the inner loop PLL to stabilize and lock before the outer loop.

        Another way of thinking about this is to recall that PLLs function as a low pass filter for phase noise arising from any source in the loop, except when they function as a high pass filter to VCO phase noise. For the OL PLL to modulate the IL’s return path without attenuation, the signal must be well within the IL BW.  

        Incidentally, if you want to estimate one quantity from another, such as frequency step rise time from PLL bandwidth, you may use this relationship:

        Tr [10%-90%] * BW [3dB] ≈ 0.35

        See for example, Howard Johnson’s discussion in the article, PLL Response Time [5].  Per his article, the time bandwidth product varies from 0.35 to 0.38, depending on whether the PLL behaves closer to a single-pole or double-pole response.

        How much faster or wider bandwidth must the inner loop be?  In mechanical engineering and process control systems, the differences in nested loop speeds can be relatively small.  A mechanical IL may be 5x to 10x faster than a mechanical OL. See for example Danielle Collins’ servo loop article in [6].  However, in timing applications, the difference in bandwidths is typically much greater. Nested dual-loop IL BWs are typically on the order of MHz, whereas OL BWs can be on the order of 10 Hz to 1 kHz, so the ratio is closer to the IL being 1000x to 100,000x faster than the OL. 

        Note that for Si538x devices, the IL BW is wide (~ 1 MHz), fixed, and optimized.  Because it is so wide, there is no jitter attenuation at the device’s XO inputs, i.e., the XA/XB pins. Therefore, we should be careful that noise and interference does not couple into the device via the XO circuit at these pins. This is why we recommend low phase noise XOs to be placed as close as possible to the device so as to minimize PCB trace lengths.

        Can this idea be extended?

        Yes, in principle. The servo control loop article cited earlier discusses a servo motor control with three nested loops, inside to outside as follows: current feedback, velocity feedback, and position feedback. Similarly, you can “triple nest loop” clock PLLs to shape the phase noise to track select input clocks with different phase noise characteristics over different frequency offsets. However, this particular approach is not utilized by the Si538x devices.  

        Conclusion

        I hope you have enjoyed this Timing 201 article. In the Part 2 follow-up post, I will discuss in more detail how to calculate the phase noise of the nested dual-loop approach using a simplified example.

        As always, if you have topic suggestions or questions appropriate for this blog, please send them to kevin.smith@silabs.com with the words Timing 201 in the subject line. I will give them consideration and see if I can fit them in. Thanks for reading. Keep calm and clock on.

        Cheers,
        Kevin

        References

        [1] W. F. Egan, Advanced Frequency Synthesis by Phase Lock. Wiley, 2011. See for example section 7.1 regarding the Two-Loop Synthesizer where two loops interact via a mixer.

        [2] Optimizing Clock Synthesis in Small Cells and Heterogeneous Networks
        https://www.silabs.com/documents/public/white-papers/Silicon-Labs-Next-Generation-DSPLL-Technology-White-Paper---June-2015.pdf

        [3] Timing 101 #11: The Case of the Noisy Source Clock Tree Part 1
        https://www.silabs.com/community/blog.entry.html/2018/10/30/timing_101_11_the-2uqO

        [4] Timing 101 #12: The Case of the Noisy Source Clock Tree Part 2
        https://www.silabs.com/community/blog.entry.html/2018/12/21/timing_101_12_the-ikzY

        [5] H. Johnson, PLL Response Time, High-Speed Digital Design Online Newsletter: Vol. 15 Issue 04,
        http://www.sigcon.com/Pubs/news/15_04.htm

        [6] D. Collins, Why is the bandwidth of a servo control loop important?, April 20, 2017, https://www.motioncontroltips.com/why-is-the-bandwidth-of-a-servo-control-loop-important/

      • Timing 201 #6: The Case of the Autonomously Resetting Clock Generator

        kgsmith | 06/161/2020 | 08:34 PM

        Introduction

        Some five years ago, a customer contacted us thinking they needed to return a clock generator device that would often go into a continuously resetting state after power-up.  We had never heard of such unusual behavior and wondered if there was anything wrong with this particular unit’s POR (Power On Reset) circuit. 

        Fortunately, the customer had a small PC board that frequently exhibited the behavior, and which they could ship to us for troubleshooting in our lab.  This enabled us to more quickly determine the root cause and verify the solution.

        It turned out that an overlooked spec for a passive component located elsewhere on the board was causing large consequences for the customer’s application. The lessons learned are generally applicable and the subject of this blog article, The Case of the Autonomously Resetting Clock Generator.

         

        BLUF (Bottom Line Up Front)

        The clock generator’s POR circuit was not at fault. In fact, it was behaving exactly as it should. Rather, an external 3.3 V regulator circuit was marginally stable. Oscillations on the 3.3 V rail could be sufficiently large to trigger autonomous resets.    

         

        Browsing the Power Supply Voltages

        The customer board took in +12 V and regulated this down to the +3.3 V and +1.8 V rails required by the Si5341 clock generator.  I used a lab power supply with pushbutton Output On/Off to provide the necessary +12 V input. This allowed me to manually and conveniently power cycle many times in order to observe and contrast a passing versus failing (continuously resetting) power-up event. The series of oscilloscope screen captures below display the 3.3 V (orange trace) at the top and the 1.8 V (blue trace) at the bottom.

        The figure below shows the nominally settled behavior of the 3.3 V and 1.8 V after a failed power-up.  The 1.8 V supply is completely accurate. However, the 3.3 V supply is clearly oscillating and even periodically dropping down to about 2.4 V, far below the POR trip threshold. 

        What about those occasions where the part successfully powers up? Per the figure below, both the 3.3 V and 1.8 V rails are at their nominal targets but the 3.3 V supply appears much noisier. This is another clue that the 3.3 V regulator circuit may be marginally stable.

        I then looked at the start-up behavior. When the device fails, the 3.3 V supply starts oscillating straight away.

        Even when the unit successfully powers up, as depicted below, the 3.3 V supply exhibits overshoot before settling down to a noisy nominal voltage.

         

        An Informative Vendor Data Sheet

        The customer was using a 500 mA LDO (Low Drop Out) regulator in a SOT-23-5 package. Reading the vendor’s data sheet, I noticed that the typical application drawing showed the output capacitor as a 2.2 uF tantalum.  Further, the data sheet explicitly stated that the output capacitor needed an ESR of about 1 Ω and that ultra-low ESR caps could cause oscillation.

        Inspecting the output cap on the customer’s board revealed that it was a ceramic capacitor. These can have an ESR with an order of magnitude less than an electrolytic capacitor. So that suggested the next experiment to try.

         

        Demonstrating the Fix

        We hacked in a 1 Ω resistor in series with the ceramic capacitor in order to emulate the approximate ESR of a tantalum capacitor. A close-up photo of the hack is shown below. The brown component in the upper part of the “elbow” is the existing capacitor. The component marked “01Y” is the 1 Ω resistor.  

        The hack was ugly but effective:

        As the resulting screen cap shows above, the 3.3 V supply is much less noisy and the start-up transient is very small and quickly damped out. After many attempts, no autonomous resets were observed, current draw was as expected, and the device always yielded output clocks.  This outcome was good enough for the customer to take over and do additional verification testing for their particular application.

         

        Some Lessons Learned

        This Timing 201 case exemplifies several lessons learned. These are listed below, going from the general to the specific.

        1. If you have a significantly puzzling problem, and can ship us a failing PC board, that can greatly speed up the overall debug process. I realize that may not always be possible due to availability, expense, intellectual property, or power/control issues. Reducing a failing board down to the lowest populated version may help mitigate some of these concerns.
        2. When troubleshooting any functional device issue, it’s always worth double-checking the supply voltages. Regulator instabilities, more subtle than this case, may even show up as increased output clock phase noise or spurs.
        3. Be aware that relatively older LDO regulators may have been designed for and require higher ESR caps than relatively newer LDO regulators.  The particular vendor used by this customer sells LDO regulators of both varieties, i.e. those that require 1 Ω ESR output stability caps and those that do not.
        4. Finally, it’s a good idea to make sure that schematics and BOMs call out exactly what LDO output capacitor is needed so that no one accidentally orders and installs the wrong type.

         

        Conclusion

        I hope you have enjoyed this Timing 201 article.  

        As always, if you have topic suggestions, or there are questions you would like answered, appropriate for this blog, please send them to kevin.smith@silabs.com with the words Timing 201 in the subject line. I will give them consideration and see if I can fit them in. Thanks for reading. Keep calm and clock on.

        Cheers,
        Kevin

      Tags

      • Wireless
      • High Performance Jitter Attenuators
      • EFR32FG22 Series 2 SoCs
      • EFR32MG21 Series 2 SoCs
      • Security
      • Bluegiga Legacy Modules
      • Zigbee SDK
      • ZigBee and Thread
      • EFR32BG13 Series 1 Modules
      • Internet Infrastructure
      • Sensors
      • Wireless Xpress BGX13
      • Blue Gecko Bluetooth Low Energy SoCs
      • Z-Wave
      • Micrium OS
      • Blog Posts
      • Low Jitter Clock Generators
      • Bluetooth Classic
      • Makers
      • Flex SDK
      • Tips and Tricks
      • timing
      • Smart Cities
      • Smart Homes
      • IoT Heroes
      • Reviews
      • RAIL
      • Simplicity Studio
      • Tiny Gecko
      • EFR32MG22 Series 2 SoCs
      • Mighty Gecko SoCs
      • Timing
      • Temperature Sensors
      • Blue Gecko Bluetooth Low Energy Modules
      • Ultra Low Jitter Clock Generators
      • General Purpose Clock Generators
      • EFR32BG22 Series 2 SoCs
      • Industry 4.0
      • Giant Gecko
      • 32-bit MCUs
      • Bluetooth Low Energy
      • 32-bit MCU SDK
      • Gecko
      • Microcontrollers
      • Jitter Attenuators
      • EFR32BG21 Series 2 SoCs
      • News and Events
      • Industrial Automation
      • Wi-Fi
      • Bluetooth SDK
      • Community Spotlight
      • Clock Generators
      • Biometric Sensors
      • General Purpose Jitter Attenuators
      • Giant Gecko S1
      • WF200
      • Flex Gecko
      • Internet of Things
      • 8-bit MCUs
      • Wireless Jitter Attenuators
      • Isolation
      • Powered Devices
      • Power

      Top Authors

      • Avatar image Siliconlabs
      • Avatar image Jackie Padgett
      • Avatar image Nari Shin
      • Avatar image lynchtron
      • Avatar image deirdrewalsh
      • Avatar image Lance Looper
      • Avatar image lethawicker

      Archives

      • 2016 January
      • 2016 February
      • 2016 March
      • 2016 April
      • 2016 May
      • 2016 June
      • 2016 July
      • 2016 August
      • 2016 September
      • 2016 October
      • 2016 November
      • 2016 December
      • 2017 January
      • 2017 February
      • 2017 March
      • 2017 April
      • 2017 May
      • 2017 June
      • 2017 July
      • 2017 August
      • 2017 September
      • 2017 October
      • 2017 November
      • 2017 December
      • 2018 January
      • 2018 February
      • 2018 March
      • 2018 April
      • 2018 May
      • 2018 June
      • 2018 July
      • 2018 August
      • 2018 September
      • 2018 October
      • 2018 November
      • 2018 December
      • 2019 January
      • 2019 February
      • 2019 March
      • 2019 April
      • 2019 May
      • 2019 June
      • 2019 July
      • 2019 August
      • 2019 September
      • 2019 October
      • 2019 November
      • 2019 December
      • 2020 January
      • 2020 February
      • 2020 March
      • 2020 April
      • 2020 May
      • 2020 June
      • 2020 July
      • 2020 August
      • 2020 September
      • 2020 October
      • 2020 November
      • 2020 December
      • 2021 January
      Silicon Labs
      Stay Connected With Us
      Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
      • About Us
      • Careers
      • Community
      • Contact Us
      • Corporate Responsibility
      • Privacy and Terms
      • Press Room
      • Investor Relations
      • Site Feedback
      • Cookies
      Copyright © Silicon Laboratories. All rights reserved.
      粤ICP备15107361号
      Also of Interest:
      • Bring Your IoT Designs to Life with Smart,...
      • IoT Hero CoreTigo Drives New Wireless Standard...
      • A Guide to IoT Protocols at Works With...