Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Official Blog of Silicon Labs

  • Show More
    Publish
    • Immediately
    • Draft
    • At scheduled date and time
     
      • Regarding the Fixed Coordinate Invalid Curve Attack and our Bluetooth Products

        Lars Lydersen | 07/212/2018 | 01:04 PM

        Last week, the Bluetooth SIG announced an update to the Bluetooth specification in response to a security vulnerability related to Secure Simple Pairing and LE Secure Connections.

        According to the SIG, researchers at the Israel Institute of Technology identified that the specification recommends, but does not require, that a device supporting these features validate the public key received over-the-air when pairing with a new device. The Bluetooth SIG has now updated the Bluetooth specification to require the validation of such keys.

        At initial connection, when pairing Bluetooth devices, the devices use mutual authentication to securely connect. The SIG has discovered the security vulnerability in the reference implementation of the public key validation during this mutual authentication (https://www.bluetooth.com/news/unknown/2018/07/bluetooth-sig-security-update).

        This means that an adversary could perform a man-in-the-middle attack during the pairing process, even for authenticated pairing schemes like numeric comparison or passkey entry. This allows the adversary to listen to and/or modify all the communication on the paired connection.

        Our Wireless Gecko products (Blue Gecko and Mighty Gecko) are not affected by this issue because they leverage the mbedTLS ECDH implementation that does not have this vulnerability. The BLE112, BLE113, BLE121LR and BLED112 modules are also not affected because they do not implement the feature that contains the vulnerability. Our BT Classic products, which include the BT111 and WTxx modules, are not affected.

        Our BT121 Bluetooth dual mode module is vulnerable to this issue. We expect to release a patch that protects against this vulnerability within 17th August 2018.

      • New Sub-GHz and BLE Solution Simplifies Industrial IoT

        Lance Looper | 06/164/2018 | 05:32 PM

        This week, we’ve introduced a Wireless Gecko software solution created to simplify industrial and commercial IoT applications using sub-GHz wireless connections by adding Bluetooth connectivity. The new hardware and software solution enables simultaneous sub-GHz and 2.4 GHz Bluetooth low energy connectivity for commercial and industrial IoT applications, such as smart metering, home and building automation, and commercial lighting.

        This is important for the industrial and commercial sectors for several reasons – for one, it’ll make it much easier for people working in these environments to set-up, control, and monitor sub-GHz IoT devices using Bluetooth low energy mobile apps.

        Sub-GHz wireless protocols are used extensively in industrial and commercial settings because many of them require a combination of energy efficiency, long battery life, and extended range for remote sensor nodes. Proprietary sub-GHz protocols allow developers to optimize their wireless solution to their specific needs instead of conforming to a standard that might put additional constraints on network implementation. With our new software solution, sub-GHz protocols can still be utilized for their benefits, but users can also easily manage the system using Bluetooth mobile apps on a variety of devices, such as tablets or smart phones.

        Sub-GHz environments are typically low-data-rate systems, such as simple point-to-point connections to large mesh networks and low-power wide area networks (LPWAN). By adding Bluetooth with low energy connectivity to wireless networks in the sub-GHz band, developers can deliver new capabilities such as faster over-the-air (OTA) updates and deploy scalable, location-based service infrastructure with Bluetooth beacons.

         

        Single Chip Reduces Cost by 40 Percent

        IoT developers stand to gain tremendous development benefits by avoiding the complexity of two-chip wireless architectures. By using a single chip with both sub-GHz and BLE connectivity, developers can simplify hardware and software development, which can speed time-to-market and reduce bill-of-materials (BOM) cost and size by up to 40 percent.

        Accenture estimates industrial IoT could add $14.2 trillion to the global economy by 2030, making the deployment potential of this solution especially massive. Any new technology developments such as this one that helps developers control and monitor industrial and commercial devices and data more easily leads to efficiency and economic gains for both businesses and the users.

        Mobile control applications are often a crucial piece of industrial and commercial automation, giving system operators a quick and easy way to control equipment. For instance, commercial lighting depends heavily on mobile devices, which control lighting on/off schedules, energy efficient modes and rules, and dimming based on occupancy using ambient light sensors. Often times, the mobile app may be the only control interface installers, designers and site managers have for project commissioning and configuration.

        Bluetooth connectivity allows the device apps and interface to be simple, which can make a difference in user adoption, as many lighting and commercial controls can be complex and difficult to manage.

        Our new solution will clearly yield impressive benefits for both developers and the users of the industrial applications. Fortunately, the new multiprotocol software is now available using Silicon Labs’ EFR32MG and EFR32BG Wireless Gecko SoCs. Check out more details here if you’re working on a product that could benefit from the solution.

         

      Tags

      • Wireless
      • High Performance Jitter Attenuators
      • EFR32FG22 Series 2 SoCs
      • EFR32MG21 Series 2 SoCs
      • Security
      • Bluegiga Legacy Modules
      • Zigbee SDK
      • ZigBee and Thread
      • EFR32BG13 Series 1 Modules
      • Internet Infrastructure
      • Sensors
      • Wireless Xpress BGX13
      • Blue Gecko Bluetooth Low Energy SoCs
      • Z-Wave
      • Micrium OS
      • Blog Posts
      • Low Jitter Clock Generators
      • Bluetooth Classic
      • Makers
      • Flex SDK
      • Tips and Tricks
      • timing
      • Smart Cities
      • Smart Homes
      • IoT Heroes
      • Reviews
      • RAIL
      • Simplicity Studio
      • Tiny Gecko
      • EFR32MG22 Series 2 SoCs
      • Mighty Gecko SoCs
      • Timing
      • Temperature Sensors
      • Blue Gecko Bluetooth Low Energy Modules
      • Ultra Low Jitter Clock Generators
      • General Purpose Clock Generators
      • EFR32BG22 Series 2 SoCs
      • Industry 4.0
      • Giant Gecko
      • 32-bit MCUs
      • Bluetooth Low Energy
      • 32-bit MCU SDK
      • Gecko
      • Microcontrollers
      • Jitter Attenuators
      • EFR32BG21 Series 2 SoCs
      • News and Events
      • Wi-Fi
      • Bluetooth SDK
      • Community Spotlight
      • Clock Generators
      • Biometric Sensors
      • General Purpose Jitter Attenuators
      • Giant Gecko S1
      • WF200
      • Flex Gecko
      • Internet of Things
      • 8-bit MCUs
      • Oscillators
      • Wireless Jitter Attenuators
      • Isolation
      • Powered Devices
      • Power

      Top Authors

      • Avatar image Siliconlabs
      • Avatar image Jackie Padgett
      • Avatar image Nari Shin
      • Avatar image lynchtron
      • Avatar image deirdrewalsh
      • Avatar image Lance Looper
      • Avatar image lethawicker

      Archives

      • 2016 April
      • 2016 May
      • 2016 June
      • 2016 July
      • 2016 August
      • 2016 September
      • 2016 October
      • 2016 November
      • 2016 December
      • 2017 January
      • 2017 February
      • 2017 March
      • 2017 April
      • 2017 May
      • 2017 June
      • 2017 July
      • 2017 August
      • 2017 September
      • 2017 October
      • 2017 November
      • 2017 December
      • 2018 January
      • 2018 February
      • 2018 March
      • 2018 April
      • 2018 May
      • 2018 June
      • 2018 July
      • 2018 August
      • 2018 September
      • 2018 October
      • 2018 November
      • 2018 December
      • 2019 January
      • 2019 February
      • 2019 March
      • 2019 April
      • 2019 May
      • 2019 June
      • 2019 July
      • 2019 August
      • 2019 September
      • 2019 October
      • 2019 November
      • 2019 December
      • 2020 January
      • 2020 February
      • 2020 March
      • 2020 April
      • 2020 May
      • 2020 June
      • 2020 July
      • 2020 August
      • 2020 September
      • 2020 October
      • 2020 November
      • 2020 December
      • 2021 January
      • 2021 February
      • 2021 March
      • 2021 April
      Silicon Labs
      Stay Connected With Us
      Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
      • About Us
      • Careers
      • Community
      • Contact Us
      • Corporate Responsibility
      • Privacy and Terms
      • Press Room
      • Investor Relations
      • Site Feedback
      • Cookies
      Copyright © Silicon Laboratories. All rights reserved.
      粤ICP备15107361号
      Also of Interest:
      • Bring Your IoT Designs to Life with Smart,...
      • Using Wi-Fi for Low Power IoT Applications
      • A Guide to IoT Protocols at Works With...