The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
 

Application engineers do not monitor this forum.
 

View General Interest Board Guidelines ›

你好,正在进行一个SERDES恢复时钟抖动消除的项目,在网上的一篇文献中有提到SI5315可以完成,具体的实现方式请参见附件图片。但是,我在SI3515的数据手册中并没有看到这种应用,不知道是否可行?附件中还有一个TI公司的CDCE62002的相同应用,但我们尝试发现效果不好,时常切换失败,不知道si5315能否实现与其相同的功能?

  • Timing
  • 32-bit MCUs
  • Discussion Forums
Unanswered
  • 你好!

     

    Si5315 是可以的,只是输入输出频率会受到一些限制,具体请参见https://www.silabs.com/documents/public/data-sheets/Si5315.pdf

    第20到28页是输入输出频率的表格,也就是说这些搭配是通过五个引脚来选取的。

     

    另外Si5315是我们上一代的产品,所以我们更推荐是新一代的高性能去抖产品 Si534x 系列。

    Si5342就是一款很适合recovered clock cleaning的芯片,价格也许会比Si5315还要便宜一点,性能强大,容易编程。

    我建议如果可能的话可以先用我们的EVB来搭一下系统,验证一下可行性。

    请问你的具体要求是什么?输入频率,输出频率,输出时钟的抖动指标?

    0
  • 感谢回复!已经联系到你们的技术支持,跟他做了进一步沟通。

    0