The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
I am working on a CP2615-EK-2 board. The DAC output of the board is connected to an Audio amplifier. when I plug the EVK USB cable into the PC, I can hear a pop noise coming from the speaker. The same noise comes after any audio stops playing. this is not a problem with the amplifier because I can hear the same noise when I plugged the headphone into the EVK audio jack. so is there any other way like changing the eI2S codec configuration from simplicity studio or by making any filter circuit?
CP2615 Audio Click and Pop noise
I am working on a CP2615-EK-2 board. The DAC output of the board is connected to an Audio amplifier. when I plug the EVK USB cable into the PC, I can hear a pop noise coming from the speaker. The same noise comes after any audio stops playing. this is not a problem with the amplifier because I can hear the same noise when I plugged the headphone into the EVK audio jack. so is there any other way like changing the eI2S codec configuration from simplicity studio or by making any filter circuit?