The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
 

Application engineers do not monitor this forum.
 

View General Interest Board Guidelines ›

Is it possible to edit/delete topic that I created?

  • Discussion Forums
  • Answered
Answered
  • you cn post 'please delete' and it wll, eventually, disappear

    0
  • Why would you want to delete your post? Do you want the question to disappear once you got your answer? To me the only reason for a post to be deleted is because it was spam or otherwise violated forum rules.

     

    To be able to edit your post is a right you have to 'earn'. See Community Ranking System and Recognition Program

    0
  • Well, in my case the forum engine has changed my topic title to something different so now the name of the topic has nothing to do with its body:

    http://community.silabs.com/t5/Timing/Can-the-LVDS-output-of-Si5330-be-AC-coupled-to-the-load/m-p/189692

     

    So I want to either be able to edit the topic title (preferable) or to delete the topic as long as there are no replies from others.

     

    0
  • Though I doubt the forum engine did any such thing, I've moved the post away for you.

    Correct Answer
    0