The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
 

Application engineers do not monitor this forum.
 

View General Interest Board Guidelines ›

 

I find C2 Debugger cable length in 8-bit MCU Knowledge Base topic. The maximum recommended cable length is six inches, but I don't know the ISA3's maximum length same it?

  • Discussion Forums
Unanswered
  • Hi,

     

    We don't have a maximum specified length for the ISA3 10-Pin Packet Trace Port (PTI) cable, but per the ISA3 Technical Specification Document TS7, the SAMTEC replacement part is FFSD-05-D-12.00-01-N, which is 12" and can be ordered online.

     

    Best,

    -Alex

    0