This article describes the process for determining if a given codec, DAC, or ADC is compatible with the CP2114, CP2614, and CP2615 Audio Bridge devices.
Notes:
For brevity, the term ‘codec’ will be used to refer to all types of external audio devices (i.e. codec, DAC and ADC devices).
It is quite common for I2S-compatible codecs to use different signal names than those used in the I2S Bus Specification. This table describes the equivalent signal names:
CP2114/2614/2615 and Codec Signal Names
I2S Specification Signal Names
LRCK, I2S_LRCLK (Left/Right Clock)
WS (Word Select)
SCK, I2S_SCK (Serial Clock)
SCK (Serial Clock)
SDOUT, I2S_SDOUT (Serial Data Output)
Transmitter SD (Serial Data)
SDIN, I2S_SDIN (Serial Data Input)
Receiver SD (Serial Data)
The following steps should be performed to determine if a given codec is compatible with the CP2114/2614/2615:
Examine the codec and CP2114/2614/2615 specifications for possible incompatibilities. (More details are provided in the following sections.)
Develop and apply the appropriate CP2114/2614/2615 configuration file(s) based on information in the codec datasheet and specific requirements of the application.
Connect the codec evaluation board to the pin headers of the CP2114/2614/2615 evaluation board (EVB) using flying wires. For best signal integrity, connections should be made using shielded coax cable or twisted pairs (signal and digital ground). To minimize ground inductance, connect multiple ground wires between the CP2114/2614/2615 and codec EVBs. All connections should be as short as possible.
Perform testing to verify functionality, proper audio performance, and conformance with the specifications of the CP2114/2614/2615 and codec datasheets, and the overall requirements of the system.
The following sections describe the functional areas that should be examined to determine compatibility of a given codec with CP2114/2614/2615 devices.
Audio Interface Format
The CP2114/2614/2615 devices operate as an audio interface master (MCLK, LRCK, and SCK are outputs). The codec must operate as an audio interface slave (MCLK, LRCK, and SCK are inputs).
The CP2114/2614/2615 devices support the following audio configurations:
Audio Functionality
16-bit
24-bit
Playback and Record
Yes
No
Playback Only
Yes
Yes
Record Only
Yes
Yes
The CP2114/2614/2615 support only I2S format; the CP2114 also supports Left-Justified format with 16 or 24 bits per sample.
Master Clock (MCLK) and Left/Right Clock (LRCK)
The CP2114 supports a sampling rate of 48 kHz only, and supports MCLK frequencies of 12.0 MHz (for 48 kHz sampling with an MCLK/LRCK ratio of 250), or 12.288 MHz (for 48 kHz sampling with an MCLK/LRCK ratio of 256). Codecs used with the CP2114 must support the 48 kHz sampling rate using either a 12.0 or 12.288 MHz MCLK.
The CP2614 and CP2615 support sampling rates of 44.1 kHz and 48 kHz, and support an MCLK frequency of 12.0 MHz only. Codecs used with the CP2614/2615 must support 44.1 kHz and 48 kHz sampling rates with a 12.0 MHz MCLK.
LRCK is derived from MCLK, so these signals are frequency- and phase-locked.
Serial Clock (SCK)
The CP2114/2614/2615 serial clock (SCK) has 24 pulses per left/right sample, even when the audio sample size is 16-bits. (An exception is the CP2114 running in 16-bit left-justified mode, in which case there are 16 SCK pulses per left/right sample.)
The SCK serial clock is ‘bursty’ (i.e. not continuous), and is low when LRCK changes state. The SCK pulses occur in between the LRCK transitions (i.e. SCK).
Although timing diagrams in many codec datasheets show a high-to-low SCK transition on each LRCK edge (as does the I2S Bus Specification), many such codecs have proven to work successfully. However, if the hardware implementation of a particular codec relies on SCK going low at LRCK transitions, the device may not be compatible.
I2C Interface (SCL and SDA)
The CP2114/2614/2615 devices provide an I2C interface for communicating with codec and other slave devices. The I2C interface can be used for:
Automatic application of initialization and shutdown sequences for any I2C slave device
Applying register settings in response to playback volume and mute commands from host
Performing user-defined I2C Write or Read operations with any I2C slave device
The CP2114/2614/2615 do not support multi-master I2C operation. There cannot be another I2C master in the system. (An exception is when the CP2614/2615 is booted in Configuration Mode to allow an external master to reprogram the CP2614/2615 configuration. In Configuration Mode the CP2614/2615 acts as an I2C slave.)
Mechanisms for Controlling Codec Mute and Volume
This table illustrates the possible methods of controlling Volume and Mute for Playback and Record:
Parameter
Control Method
CP2114
CP2614/2615
Playback Volume Control
I2C Register bitfield
Yes
Yes
Playback Mute Control
I2C Register bitfield
Yes
Yes
GPIO Output
Yes
Yes
Specific volume-register value
Yes
No
Set DAC samples to zero
Yes
No
Record Mute Control
Set ADC samples to zero
Yes
Yes
The CP2114/2614/2615 devices provide a mechanism to linearly map audio playback volume settings (in dB) to the appropriate register values. The devices support signed and unsigned register values, but the relationship between volume setting (in dB) and register setting must be directly proportional (i.e. register value increases as volume setting increases). An inversely proportional relationship (i.e. register value decreases as volume setting increases) is not supported.
Acoustic Echo Cancellation (AEC)
If the system requires acoustic echo cancellation, a 48 or 49.152 MHz external clock must be used to drive the CP2114 EXTCLK pin. (The CP2614/2615 devices do not support the use of an external clock.)
No. CP2400/2 devices have a 4-wire Serial Peripheral Interface (SPI) which provides access to the internal registers and memory. The active-low slave-select (NSS) signal allows support for multiple slave devices on a single bus. It is also used to detect the start and end of a SPI transfer for CP2400/2, and should be connected to the SPI master instead of connection to a static low level signal, e.g. GND. The SPI transaction ends when NSS is de-asserted.
The last two bytes of this configuration are a 'fletcher' checksum of the rest of the bytes of the array. That checksum is described in this wikipedia article:
Additionally, two implementations of this algorithm are included below.
First, the 'C' implementation:
// Taken from Wikipedia https://en.wikipedia.org/wiki/Fletcher%27s_checksum// Must use generic pointer since function is called on XDATA and CODE spaces.uint16_t fletcher16(uint8_t*dataIn,uint16_t bytes){uint16_t sum1 =0xff, sum2 =0xff;uint16_t tlen;while(bytes){
tlen = bytes >=20?20: bytes;
bytes -= tlen;do{
sum2 += sum1 +=*dataIn++;}while(--tlen);
sum1 =(sum1 &0xff)+(sum1 >>8);
sum2 =(sum2 &0xff)+(sum2 >>8);}/* Second reduction step to reduce sums to 8 bits */
sum1 =(sum1 &0xff)+(sum1 >>8);
sum2 =(sum2 &0xff)+(sum2 >>8);return sum2 <<8| sum1;}
In AN721SW.zip there exist standalone manufacturing tools that can be used to program CP21xx devices. This is described in section 4.1 of the AN721 application note. Attached to this article is a zip file that contains the default configurations for all programmable CP21xx devices:
In AN434, the reports list lists two I2C reports: I2C Read (0x7E) and I2C Write (0x7D). Can I use these HID reports to use the CP2114 as an I2C pass-through device from the host to the attached codec?
Answer
Yes. However, these two reports are only available on the CP2114-B02 devices. CP2114-B01 devices do not have this capability.
I am using the CP2615 Evaluation Kit and changed the "terminal input type" from "line" to "microphone" in Xpress Configurator, but I am unable to record anything using the mic input. How to I use the mic input on this board?
Answer
The "terminal input type" parameter only changes USB descriptors on the CP2615. These do not change the ADC input on the Tempo TSCS25A3X1NDGXZAX codec.
To change the ADC input of the codec from the line to mic:
1. Write 0x40 to codec address 0x0C and 0x0D as shown below.
2. If using a Rev 1.0 board, connect the mic connector (J10) ground to the analog ground.
What is the spacing of the pins on the CP2102N Mini Evaluation Kit (CP2102N-MINIEK)?
Answer
There are two rows of pins on the CP2102N-MINIEK. On each row, the pins are 0.1" apart on center to the pins. The distance between the two rows is 0.6" on center to the pins. This board can also used on a standard breadboard with 0.1" pitch.
Interface Knowledge Base
Global Call Address
Determining Codec/ADC/DAC compatibility with CP2114/CP2614/CP2615 devices
This article describes the process for determining if a given codec, DAC, or ADC is compatible with the CP2114, CP2614, and CP2615 Audio Bridge devices.
Notes:
CP2114/2614/2615 and Codec Signal Names
I2S Specification Signal Names
LRCK, I2S_LRCLK (Left/Right Clock)
WS (Word Select)
SCK, I2S_SCK (Serial Clock)
SCK (Serial Clock)
SDOUT, I2S_SDOUT (Serial Data Output)
Transmitter SD (Serial Data)
SDIN, I2S_SDIN (Serial Data Input)
Receiver SD (Serial Data)
The following steps should be performed to determine if a given codec is compatible with the CP2114/2614/2615:
The following sections describe the functional areas that should be examined to determine compatibility of a given codec with CP2114/2614/2615 devices.
Audio Interface Format
The CP2114/2614/2615 devices operate as an audio interface master (MCLK, LRCK, and SCK are outputs). The codec must operate as an audio interface slave (MCLK, LRCK, and SCK are inputs).
The CP2114/2614/2615 devices support the following audio configurations:
Audio Functionality
16-bit
24-bit
Playback and Record
Yes
No
Playback Only
Yes
Yes
Record Only
Yes
Yes
The CP2114/2614/2615 support only I2S format; the CP2114 also supports Left-Justified format with 16 or 24 bits per sample.
Master Clock (MCLK) and Left/Right Clock (LRCK)
The CP2114 supports a sampling rate of 48 kHz only, and supports MCLK frequencies of 12.0 MHz (for 48 kHz sampling with an MCLK/LRCK ratio of 250), or 12.288 MHz (for 48 kHz sampling with an MCLK/LRCK ratio of 256). Codecs used with the CP2114 must support the 48 kHz sampling rate using either a 12.0 or 12.288 MHz MCLK.
The CP2614 and CP2615 support sampling rates of 44.1 kHz and 48 kHz, and support an MCLK frequency of 12.0 MHz only. Codecs used with the CP2614/2615 must support 44.1 kHz and 48 kHz sampling rates with a 12.0 MHz MCLK.
LRCK is derived from MCLK, so these signals are frequency- and phase-locked.
Serial Clock (SCK)
The CP2114/2614/2615 serial clock (SCK) has 24 pulses per left/right sample, even when the audio sample size is 16-bits. (An exception is the CP2114 running in 16-bit left-justified mode, in which case there are 16 SCK pulses per left/right sample.)
The SCK serial clock is ‘bursty’ (i.e. not continuous), and is low when LRCK changes state. The SCK pulses occur in between the LRCK transitions (i.e. SCK).
Although timing diagrams in many codec datasheets show a high-to-low SCK transition on each LRCK edge (as does the I2S Bus Specification), many such codecs have proven to work successfully. However, if the hardware implementation of a particular codec relies on SCK going low at LRCK transitions, the device may not be compatible.
I2C Interface (SCL and SDA)
The CP2114/2614/2615 devices provide an I2C interface for communicating with codec and other slave devices. The I2C interface can be used for:
The CP2114/2614/2615 do not support multi-master I2C operation. There cannot be another I2C master in the system. (An exception is when the CP2614/2615 is booted in Configuration Mode to allow an external master to reprogram the CP2614/2615 configuration. In Configuration Mode the CP2614/2615 acts as an I2C slave.)
Mechanisms for Controlling Codec Mute and Volume
This table illustrates the possible methods of controlling Volume and Mute for Playback and Record:
Parameter
Control Method
CP2114
CP2614/2615
Playback Volume Control
I2C Register bitfield
Yes
Yes
Playback Mute Control
I2C Register bitfield
Yes
Yes
GPIO Output
Yes
Yes
Specific volume-register value
Yes
No
Set DAC samples to zero
Yes
No
Record Mute Control
Set ADC samples to zero
Yes
Yes
The CP2114/2614/2615 devices provide a mechanism to linearly map audio playback volume settings (in dB) to the appropriate register values. The devices support signed and unsigned register values, but the relationship between volume setting (in dB) and register setting must be directly proportional (i.e. register value increases as volume setting increases). An inversely proportional relationship (i.e. register value decreases as volume setting increases) is not supported.
Acoustic Echo Cancellation (AEC)
If the system requires acoustic echo cancellation, a 48 or 49.152 MHz external clock must be used to drive the CP2114 EXTCLK pin. (The CP2614/2615 devices do not support the use of an external clock.)
CP2400/2 SPI NSS Pin Connection
Fletcher Checksum for CP2102n configuration array
Default configurations for CP21xx command-line programming tools
CP2114: I2C commands through HID interface
CP2615 Evaluation Kit Mic Input
CP2615 Evaluation Kit Schematic, BOM, Layout
CP2102N-MINIEK Pin Spacing
Thermal resistance of the CP2103