I am using Si83414AAA-IF with 24V VDD2 power supply. When running, Si83414AAA-IF has a temperature of more than 45 degrees Celsius although no channels are enabled. With the VDD2 12V power supply, the temperature is close to 40 degrees Celsius. Ambient temperature 25 degrees C.
Can you confirm for me that the temperature is normal?
Why does it have such a high temperature when in operation?
I attach the PCB photo below.
Isolation
Discussion Forums
Answered
Answered
Sir or Madam:
I believe you also entered a SF ticket for this question, but to address your question here just in case, yes, this is normal operation.
Please follow up with additional questions via the Sales Force Ticket you created.
High operating temperature Si83414AAA-IF
I am using Si83414AAA-IF with 24V VDD2 power supply. When running, Si83414AAA-IF has a temperature of more than 45 degrees Celsius although no channels are enabled. With the VDD2 12V power supply, the temperature is close to 40 degrees Celsius. Ambient temperature 25 degrees C.
Can you confirm for me that the temperature is normal?
Sir or Madam:
I believe you also entered a SF ticket for this question, but to address your question here just in case, yes, this is normal operation.
Please follow up with additional questions via the Sales Force Ticket you created.
Apps Support