According to the EFR32xG21 reference manual, "User Data is locked by default, and all User Data write and erase operations must be performed via the SE" (Section 6.3.11.2 Flash Lock)
Please refer to our example using the SE API from the peripheral examples repository
BGM210P issue writing in UD flash
Hello,
I'm trying to write 8 Bytes in UserData flash but function MSC_ErasePage always return mscReturnLocked.
Setup :
Code :
Thanks in advance for your help.
Regards,
Gabriel
Hello Gabriel,
According to the EFR32xG21 reference manual, "User Data is locked by default, and all User Data write and erase operations must be performed via the SE" (Section 6.3.11.2 Flash Lock)
Please refer to our example using the SE API from the peripheral examples repository
Thanks for pointing that out.
It works well.
Regards,
Gabriel