No I am working on custom board which included controller EFM32TG11B520F128GQ48 controller
Is there any method to check whether my bootloader is erased or not?
Dipak Garasiya
0
You can dump the flash content with Simplicity Commander.
Also try to upload the screenshot when the issue happen.
0
That is nothing problem when i flash hex file of project to controller with Simplicity Commander . it successfully flashed to controller
but when i run program after removing debugger it doesn't work
it works ok when debugger is connected
Dipak Garasiya
0
As I said previously, you need provide more information as I requested previously.
If this is custom board, please also upload the schematic and the code you are trying to program into the device.
0
Are you going into a low energy mode (EM2/3)? Note that, when the debugger is connected, the device does not actually fully go into these modes, and instead goes into an equivalent of EM1.
0
I have uplaoded my schematic of custom board and zip file of program which is not working on controller
I want to clear that both PF0 and PF1 has external pull-up.
Dipak Garasiya
0
there is problem to upload file recently.
you can try send the attachment to me via email.
0
i am unable to attach my pdf and zip file alongwith post . how can i do it. for schematic and program
0
please share your E-Mail Id
0
I suggest you try the simple example like blink to see if you still have the issue first.
program works only when debugger is connected
Hello
I am working on controller EFM32TG11B520F128GQ48 .
while I am working i found strange issue with controlller . it only works when debugger is connected otherwise isn't working
Dipak Garasiya
Which IDE you are using?
Are you working on the Silabs EFM32TG11 STK?
I am wondering if you have the bootloader erased.
https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2018/10/02/recovering_an_efm32g-S64B
I am using Simplicity Studio .
No I am working on custom board which included controller EFM32TG11B520F128GQ48 controller
Is there any method to check whether my bootloader is erased or not?
Dipak Garasiya
You can dump the flash content with Simplicity Commander.
Also try to upload the screenshot when the issue happen.
That is nothing problem when i flash hex file of project to controller with Simplicity Commander . it successfully flashed to controller
but when i run program after removing debugger it doesn't work
it works ok when debugger is connected
Dipak Garasiya
As I said previously, you need provide more information as I requested previously.
If this is custom board, please also upload the schematic and the code you are trying to program into the device.
I have uplaoded my schematic of custom board and zip file of program which is not working on controller
I want to clear that both PF0 and PF1 has external pull-up.
Dipak Garasiya
there is problem to upload file recently.
you can try send the attachment to me via email.
Let us address the issue with support case.
I think you can upload your schematic file now.
The issue (failure to upload image and other file along with post) was fixed.