Question

The Lock bits description section (6.3.2) in the reference manual of EFM32PG12 states the following about the bankswitch disable bit -

 

Capture.PNG

 

At what position is the Bankswitch disable bit?

Answer

The bankswitch disable bit is bit 0 of the configuration word One. If the value of this bit is 1, bankswitching is disabled. 

  • Knowledge Base Articles
  • 32-bit MCUs