My views are my own and do not necessarily represent the views of Silicon Labs
0
Hi Delu,
Thanks for reply,
Silicon described the driver:
The Silicon Labs Interrupt Driver is an example Universal Serial Bus (USB) device driver for use with the Silicon Labs C8051F320 target board and USB_INT example device firmware. The device driver is a Windows® Driver Model architecture driver which is compatible with Windows 98, 2000 and XP operating systems. The driver fully supports Plug and Play (PnP) and Power Management (PM). Refer to the DDK documentation to understand the handling of PnP and PM features and implementations. The Microsoft Windows Driver Development Kit is available free of charge from Microsoft® at http://www.microsoft.com/whdc/ddk/winddk.mspx. The USB device used for this sample is the Silicon Labs C8051F32x evaluation board programmed with the USB Interrupt example provided in the examples directory by default in the SiLabs\MCU\Examples\C8051F32x\c\USB_INT directory.
We had do some modification for our own user,but it can't work for Win10 64 bit. How can I get the right driver for WIN10?
0
As far as I remember these sample use WinUSB driver from windows.
Do you mean you need a old driver maybe named SiUSBXp from Silabs?
My views are my own and do not necessarily represent the views of Silicon Labs
0
In fact,I need the new version of that driver,who can install for WIN10, and I need the driver source to debug.
Thanks!
0
Could you create a ticket in our technical support portal as bwlow link?
c8051f320 usb_int WIN10
Hi all,
I need the driver of C8051F320 for Win10 64 Bit(USB_INT), and the source code of the driver.
Regards,
xa_LinNa
Hi xa_LinNa
Do you mean the USBXpress (rather than USB_INT) in below link?
http://www.silabs.com/products/mcu/Pages/8-bit-microcontroller-software.aspx#ide
If you need the source code, suggest create a ticket in
http://www.silabs.com/support/Pages/default.aspx
My views are my own and do not necessarily represent the views of Silicon Labs
Hi Delu,
Thanks for reply,
Silicon described the driver:
The Silicon Labs Interrupt Driver is an example Universal Serial Bus (USB) device driver for use with the Silicon
Labs C8051F320 target board and USB_INT example device firmware. The device driver is a Windows® Driver
Model architecture driver which is compatible with Windows 98, 2000 and XP operating systems.
The driver fully supports Plug and Play (PnP) and Power Management (PM). Refer to the DDK documentation to
understand the handling of PnP and PM features and implementations. The Microsoft Windows Driver
Development Kit is available free of charge from Microsoft® at http://www.microsoft.com/whdc/ddk/winddk.mspx.
The USB device used for this sample is the Silicon Labs C8051F32x evaluation board programmed with the USB
Interrupt example provided in the examples directory by default in the
SiLabs\MCU\Examples\C8051F32x\c\USB_INT directory.
We had do some modification for our own user,but it can't work for Win10 64 bit. How can I get the right driver for WIN10?
As far as I remember these sample use WinUSB driver from windows.
Do you mean you need a old driver maybe named SiUSBXp from Silabs?
My views are my own and do not necessarily represent the views of Silicon Labs
In fact,I need the new version of that driver,who can install for WIN10, and I need the driver source to debug.
Thanks!
Could you create a ticket in our technical support portal as bwlow link?
http://www.silabs.com/support/Pages/default.aspx
new post in chinese forum:
http://community.silabs.com/t5/ChineseForum/c8051f320-usb-driver-for-WIN10/m-p/168111#U168111