8-bit Knowledge Base

    Publish
     
      • 复位时 Port I/O 状态

        delu | 02/42/2018 | 12:32 AM

        问题

        端口I/O引脚在设备复位时状态是怎样的?

         

        答案

        在任何复位源(比如把复位引脚拉低)确认阶段,所有端口I/O引脚默认配置为数字输入且弱上拉状态。

         

        English version: Port I/O State at Reset

      • Keil uVision查看不同存储器的值

        yucheng | 02/39/2018 | 11:45 PM

        问题

        Keil uVision debug MCU时,如何查看直接寻址的片内RAM、间接寻址的片内RAM、扩展的外部RAM和代码存储空间 ?

        答案

        使用Keil uVision对MCU进行debug时,可通过其memory窗口查看不同存储器的值。

         

         11.png

         

        以debug EFM8UB2为例,

        查看直接寻址的片内RAM时,在memory窗口输入D:0x00, 即可以查看从0x00地址开始的直接寻址的片内RAM的值

        12.png

         

        查看间接寻址的片内RAM时,在memory窗口输入I:0x00

        13.png

         

        查看扩展的外部RAM,在memory窗口输入X:0x0000

        14.png

         

        查看代码存储区域时,在memory窗口输入C:0x0000

        15.png

         

        建议在debug时使用Silabs推出的Simplicity Studio V4, 其界面更为直观,debug更为高效。

      • MCU Example Code

        delu | 02/39/2018 | 10:25 PM

        Question

         


        Where can I find example code for the C8051xxxx MCU?



         

        Answer

         


        Example code for Silicon Labs's MCUs is available in two main locations. 

        The first is the Application Note webpage:
        https://www.silabs.com/products/mcu/Pages/ApplicationNotes.aspx

        On the Application Note webpage, the example code is organized by topic, such as ADC or UART.  Check the beginning of the application note to determine if the application note is applicable to your MCU.

        Example code is also part of the Silicon Labs IDE.  The Silicon Labs IDE is available for download at:
        https://www.silabs.com/products/mcu/Pages/SoftwareDownloads.aspx

        If the IDE is installed to the default directory, the example code is installed at:
        C:\SiLabs\MCU\Examples

        In the Examples directory, the example code is organized by the MCU family.  There are over 1000 pieces of example code currently available in this directory.

         

      • Ethernet Examples

        delu | 02/39/2018 | 08:20 PM

        Question

        Where can I find Ethernet examples for Silicon Labs MCUs?

         

        Answer

        Ethernet examples for the 'F12x and the 'F34x are attached to this article.  These are the lowest layer, hardware-level routines intended to be interfaced with a Ethernet stack.

      • Is it possible to change the resistor value between XTAL1 and XTAL2 ?

        yucheng | 01/25/2018 | 04:09 AM

        Most of the C8051 devices include an external oscillator drive circuit to driver an external crystal, ceramic resonator, capacitor, or RC network.

        For a crystal or ceramic resonator configuration, the crystal/resonator must be wired across the XTAL1 and XTAL2 pins as shown in the figure below. And a 10M ohm resistor must be wired across the XTAL2 and XTAL1 pins for the crystal/resonator configuration.

        The 10 M ohm resistor between XTAL1 and XTAL2 is required to provide proper DC bias to the internal crystal driver. And the parallel impedance (10M ohm) decides the loop gain. Having a larger impedance is usually desired because it will increase the loop gain, and hence reduce start up time and increase negative impedance. So it shouldn't try to reduce this 10M ohm impedance.

        With regard to the unstable or unable to start up oscillation, please check the items below one by one.

        1. Review the PCB layout:

        Crystal oscillator circuits are quite sensitive to PCB layout.

        • The crystal should be placed as close as possible to the XTAL pins on the device.
        • The traces should be as short as possible and shielded with ground plane from any other traces which could introduce noise or interference.
        • Place the loading capacitors close to the crystal pins to minimize loop area.

        AN203 provided a good starting point in the design and layout of a PCB, and the methods presented in this application note should be taken as suggestions.

        2. Check the capacitors value connected to the crystal.

        The capacitors shown in the external crystal configuration provide the load capacitance required by the crystal for correct oscillation. These capacitors are "in series" as seen by the crystal and "in parallel" with the stray capacitance of the XTAL1 and XTAL2 pins.

        The desired load capacitance CL depends upon the crystal and the manufacturer. Refer to the crystal data sheet when completing these calculations below.

        The equation for determining the load capacitance for two capacitors is as follows:

        C is the capacitor value connected to the two crystal leads, in general, will connect a same capacitor on each lead. CS is the total stray capacitance of the PCB, and the stray capacitance for a typical layout where the crystal is as close as possible to the pins is 2-5 pF per pin.

        For example, a tuning-fork crystal of 25 MHz has a recommended load capacitance of 12.5 pF. With a stray capacitance of 3 pF per pin (6 pF total), the 13 pF capacitors yield an equivalent capacitance of 12.5 pF across the crystal.

        12.5 pF = C/2 + 6

        C = 13 pF

        3. Choose a reasonable driver level

        Please refer to the KB below to choose a reasonable driver level.

        https://www.silabs.com/community/mcu/8-bit/knowledge-base.entry.html/2017/03/31/choosing_c8051_cryst-cMgw

        The KB describe how to specify the XFCN to issue a reasonable crystal driver current considering the required Drive Level (DL) and Equivalent Series Resistance (ESR) of the crystal rather than only considering the frequency.

        4. Measure the actual driver level on board

        If the crystal still unstable or cannot start up after checking the items above, you should measure the actual driver level on board (Crystal vendor should be able to provide the test report). If the measured driver level is way larger than the maximum specification, the crystal will be over-driven and may result to the crystal circuit not working, and the crystal operational lifetime will be reduced.

        The recommended method is adding a series resistance Rd to the crystal to reduce the driver level.

         

      • SMBus Timing Performance Explained

        Alan_S | 12/339/2017 | 05:58 PM

        Why does the datasheet say the Fast Mode (400 KHz Class) SMBus has a maximum operating frequency of 255 kHz?

         

        The SMBus peripheral is internally clocked at 3 times the target bit rate and generates clock low from 1 clock cycle and clock high from 2 clock cycles.

         

        The SMBus 400 kHz fast speed specifies clock low must be at least 1.3 us.  So 1/(3x1.3us) = 256 kHz.  If you set the SCL frequency to higher than 256 kHz, then the clock low time will be less than 1.3 us and violate the spec.

         

        In practice, many I2C devices will work fine above 256 kHz, but the device will be in violation of the timing requirements, so full compatibility can't be guaranteed for strict systems.

      • How does the offset DAC on the C8051F35x function?

        JohnB | 12/335/2017 | 03:39 PM

        I am trying to use ADC on the C8051F35x and am having problems figuring out how the offset DAC works.

        First of all, I am not sure if the offset DAC is added to or subtracted from the AIN+ and AIN- inputs such that it has the effect of level-shifting, is applied to only one input, or even if its doing the opposite on both inputs (half the value subtracted from AIN+ and half value added to AIN-, which would cancel any offset completely.

        Also, application note AN217, which has the same block diagram as the 'F35x datasheet...

        ...shows that the offset should be applied before the gain, but in my tests it seems to be done afterwards.

        From what I can tell, the offset voltage is substracted after the amplification. Is this expected behavior, or am I doing something wrong?

         

        As the customer has noted, there appears to be a notable difference in how the offset DAC behaves relative to the PGA, and, in this case, the customer is correct: the offset DAC operates after the PGA. So, for starters, the block diagram above should be modified as follows:

        Furthermore, consistent with the customer's experiments, the ODAC output is subtracted from AIN+ and added to AIN- as a signed value, where bit 7 and bits [6:0] of the ADC0DAC register represent the sign value (0 = positive, 1 = negative) and the magnitude, respectively.

      • Isochronous transfer support in USB Peripheral Driver Library

        Alan_S | 11/332/2017 | 06:03 PM

        When trying to do isochronous transfers with the USB Peripheral Driver Library, you may notice that the library only supports isochronous transfers on Endpoint 3 even though the device's datasheet says endpoints 1-3 support isochronous transfers.

        The device does support isochronous transfers on endpoints 1 through 3, but the library was only designed to support isochronous transfers on endpoint 3 by default. All Silicon Labs designs use endpoint 3 for isochronous transfers, so the library was built around this as well as with the idea of keeping the code simple in mind. The library can be modified to support isochronous on other endpoints, but the library does not support this out of the box.

      • Current Consumption Examples?

        Alan_S | 11/331/2017 | 06:23 PM

        I am trying to reproduce the current consumption numbers specified in the datasheet of an EFM8 device. How do I make sure that I am using the same settings as the numbers in the datasheet?

        Provided with Simplicity Studio is a set of software examples that demonstrate how to use the device's various peripherals. One of these examples is PowerModes and shows how to put the device into its various low power states. In Simplicity Studio, this code is listed under Software Examples when you have your device selected.

      • TestPanel example in USBXpress SDK does not work?

        LiuJiehui | 11/321/2017 | 05:06 AM

        Question

        While running the TestPanel example which included in the USBXpress 4 SDK v4.0.3 on C8051F340 MCU, the device can be enumerated as a USBXpress Device viewing from the Windows Device Manager, however, it failed to start the Host application TestPanel.exe, what would cause the issue as below?

         

        Answer

        This is caused by incorrect USBXpress driver version installed on your machine if you are not using the USBXpress driver that is included in the same SDK version.

        To solve the issue, uninstall the existing driver of the USBXpress Device, and then re-install the corresponding driver included in the USBXpress SDK where you are running the USBXpress example.

        For the USBXpress SDK v4.0.3 mentioned above, the driver version is 4.0.0.0 with driver date of 4/8/2013.