Member | Action | Date |
---|---|---|
|
Posted
SI4684 : Unable to retrieve Slideshow Content associated to a service on
Forum
Hi, I'm currently working on a Si4684 and I try to retrieve the content of a SLS. Here is the configuration of my sample multiplex, which is working on DAB Player on Windows (which shows SLS and DLS+) and on a several other receivers : Ensemble 0xFFB2, Label: 'Local Test', ShortLabel: 'LocalTst', LTO: +60 min, ECC: 0xE1, NumServices: 1 I can't get slideshow data via the GET_DIGITAL_SERVICE_DATA registry. When I call this registry, while the service is playing: i got audio, and it only returns DLS and DLS+ tags informations. No trace of SLS. When i call DAB_GET_COMPONENT_INFO, i can see that there is 1 UserApp of type 0x2 (so MOT SLS) and its data is 0C3C. So the SLS is well flagged. Before that, I took care to activate MOT SLS and DLS reception via the DAB_XPAD_ENABLE registry. How to enable extraction of SLS via the GET_DIGITAL_SERVICE_DATA registry ? FYI, i got the DAB FW 5.0.9. Thanks Fabien |
Feb 19 2020, 4:04 PM |