Member | Action | Date |
---|---|---|
![]() |
Posted
CP210x VCP Driver (v6.0.1) for macOS Big Sur v11.2.3 not installing on
Interface Device Forum
Hello,
Previously I had issues with installing v6.0 of the CP210x VCP drivers on Big Sur v11.1. Original post - https://www.silabs.com/community/interface/forum.topic.html/new_cp210x_vcp_driveronbigsur-5icm
Now, after updating to 11.2.3 the drivers are no longer installed in my machine and I get another error when trying to install the drivers I had received from the above post.
Attached is the text from the error screen... |
41 days ago |
![]() |
Replied
to
New CP210x VCP Driver on Big Sur
Nam, That seemed to work without issue! Thank you! But I wonder if it had something to do with a similar issue with a beta version of a VPN app I was also trying to install. I ended up uninstalling Sophos Home from my iMac and then I was able to successfully install that. ???? Thank you for your help! |
Dec 24 2020, 12:48 PM |
![]() |
Selected an answer for
New CP210x VCP Driver on Big Sur
Hi Jeff2A, Thank you for posting your issue. However, we haven't be able to reproduce your issue on our side yet. Our R&D team try to update the driver which give a small tweak to see if it can work on your side. You can find the updated driver in the attachment. Please give it a try and let me know about your result. Regards, |
Dec 24 2020, 12:45 PM |
![]() |
Posted
New CP210x VCP Driver on Big Sur on
Interface Device Forum
Upon installing the new CP210x VCP Driver downloaded this morning on Big Sur macOS 11.1 (on a 2017 27" iMac) I get this error:
This is the text that pops up from Apple's error window: Process: CP210xVCPDriver [80747] Date/Time: 2020-12-23 07:30:17.537 -0500 Sleep/Wake UUID: FE892419-69A4-42E8-80D2-C824490ABAB9 Time Awake Since Boot: 51000 seconds System Integrity Protection: enabled Crashed Thread: Unknown Exception Type: EXC_CRASH (Code Signature Invalid) kernel messages: Backtrace not available Unknown thread crashed with X86 Thread State (64-bit): Unknown thread instruction stream not available. Unknown thread last branch register state not available.
Model: iMac18,3, BootROM 429.60.3.0.0, 4 processors, Quad-Core Intel Core i5, 3.5 GHz, 32 GB, SMC 2.41f2
Any idea?
Thanks. |
Dec 23 2020, 1:07 PM |