Member | Action | Date |
---|---|---|
|
Posted
Z-Wave Controller CLI Scripting on
Z-Wave Wireless Forum
I would like to setup an automatic test system for a z-Wave device which is base on the ZGM130s. Basically I would like to be able to add the device to the network and interact with it in some form of scriptable way. And it needs to run in a linux environment. Is there any way that is achievable?
Show more
Can I interface the UZB-7 dongle easily with some command line application? |
Oct 01 2020, 12:49 PM |
|
Replied
to
How to OTA a co-processor via Z-Wave
This article is very helpful, thank you! I have some questions though:
|
Sep 29 2020, 8:30 AM |
|
Replied
to
OTA using Z wave for other processor
We are having a very similar case where we need to be able to update a main Atmel MCU. I would also like to know if it is possible and possibly how this can be handled?
Show more
|
Sep 22 2020, 2:23 PM |