Member | Action | Date |
---|---|---|
![]() |
Replied
to
Does Ember offer a SPI or I2C driver that I can use with the EM35x HAL?
Please can anyone share the I2C bus driver code for EM35x? |
Oct 28 2017, 2:07 PM |
![]() |
Replied
to
Does Ember offer a SPI or I2C driver that I can use with the EM35x HAL?
I installed Thread 1.0.2 for EM35x Dev kit and I dont find the I2C Driver in hal/micro/cortexm3/bootloader folder.
|
Oct 28 2017, 2:07 PM |
![]() |
Posted
Commissioning second Border Router in Thread network on
Forum
Hi,
I have two Silabs BRs RD-0004-0101. First BR runs ext. Commissioner & successfully adds Thread devices to Network and then I want to add second BR. Current BR code does not allow setting of Joining key and entering the already existing Thread network.
Please tell me that if it is even possible to add second BR using current BR software? if Yes then how?
Thanks.
Best Regards, Zeshan
|
Oct 28 2017, 1:48 PM |
![]() |
Replied
to
Multiple border router
Hallo Konrad,
Is this feature (Using Multiple Border Routers in Thread net) is implemented yet? Is it possible now to commission second BR? Thanks.
BR Zeshan
|
Oct 28 2017, 1:37 PM |