Member | Action | Date |
---|---|---|
|
Replied
to
Unstable connection in 0dBm and 1dBm in Throughput test
Hi Anna, sorry for reply you late. Do you have another radio board for a try? We don't have MGM210P022 on hand, so use BRD4180A/BRD4181A for test, can not reproduce the issue here. If you still need help on this issue, it would be better if you can open a ticket on our Salesforce platform.
Show more
|
3 days ago |
|
Replied
to
BGM12S Single push button to Sleep and wakeup
Could you share the more detail part Number information and what do you want? Here are some example code you can reference. https://github.com/SiliconLabs/peripheral_examples/tree/master/series1 https://github.com/SiliconLabs/peripheral_examples/tree/master/series1/gpio https://github.com/SiliconLabs/peripheral_examples/tree/master/series1/emu/ |
3 days ago |
|
Replied
to
Problem with NCP Target and Deep Sleep EM2 on Bluetooth Gecko v3.1
Have you test the demo prebuild hex file with BGTool, it works for me. If not, could you have a try? To reproduce the issue, do we need to do some customize?
Show more
|
39 days ago |
|
Replied
to
Error in data sending through notify
Could you do some more test? 1) Test with 2 WSTK boards. 2) Test with other phone App, EFR connect. |
45 days ago |
|
Replied
to
BGM11S12F256GA -> Which EF32 Part Number?
EFR32BG1B232F256M48 Refer to this link. |
45 days ago |
|
Replied
to
Static OOB authentication in Bluetooth Mesh SDK 2.0.0.0 and Simplicity Studio 5
Will study and check you the code, update here when I got some finding.
Show more
|
50 days ago |
|
Replied
to
EFR32BG22 flashload error with IAR
The project file create by SSv4 or SSv5? Need to reproduce for check.
Show more
|
50 days ago |
|
Replied
to
Displaying Battery Level on Android notification bar
It looks like handle by Android system side, will keep study on it, if got findings will update here.
Show more
|
50 days ago |
|
Replied
to
nearest neighbor discovery
rail_getRssi() may help, but it will not always works. You may need to consider the tx power on each node or the obstacle between nodes.
Show more
|
59 days ago |
|
Replied
to
Auto-ACKing functionality
Got an internal discuss, we don't think this is an issue. That way RAIL can examine the header and properly interpret the packet as an ACK packet and not a message packet, this should do in application level.
Show more
|
Dec 08 2020, 1:23 AM |