Member | Action | Date |
---|---|---|
|
Replied
to
IAS Zone device does not announce in Zigbee network
I also met the same problem. Is there any result so far? I'm not sure if it's a device or gateway problem. |
Oct 28 2020, 2:19 AM |
|
Posted
zipgateway7.14 /demo/controller_app mips, can add and remove devices, but can not control switch on/off for switch devices. on
Z-Wave Wireless Forum
Problem: Can add and remove devices, but can not control switch on/off for switch devices. Device: ZGM130S, ..\v5\developer\sdks\gecko_sdk_suite\v3.0\protocol\z-wave\Apps\bin\ZW_SerialAPI_Controller_7.14.1_241_ZGM130S_REGION_CN.hex zipgateway: C:\SiliconLabs\SimplicityStudio\v5\developer\sdks\zwave\zip_gateway\v7.14.1\Source\zipgateway-7.14.01-Source.tar zware: C:\SiliconLabs\SimplicityStudio\v5\developer\sdks\zwave\zware\v7.14.1\REL14434_7.14.01\src\zware.tar Runing Platform: mips_32 Little-Endian, using zipgateway and ~/demo/controller_app for test, run the same board(locally). Compile platform: Ubuntu18.04 64 DIR:
Zipgateway:
ZWARE:
I changed the makefile to support my hardware:
After put zipgateway and controller_app into my hardware platform. I can add and remove device, but can not control it. I also put 'l' and 'd' in zipgateway after controll device fail.
|
Sep 25 2020, 2:56 AM |
|
Replied
to
Unsolicited report using binary switch doesn't work with z-ware library and zipgateway (sdk 7.11.0)
The problem is same on my platform, I'm not sure it is an ip issue, for I can recove report after 10~20S, while the local button pressed.The line "ApplicationCommandHandler 6->1 class 0x20 cmd 0x03 size 3" indicate that the gateway got massge from sub-device, but DTLS timeout at next lines. After 10~20S. The line "node_input_queued: Packet for DTLS_PORT uip_len: 77" printed., I got message from gateway. The app and gateway run the same board, using IPV6 UDP communication. |
Sep 21 2020, 6:00 AM |
|
Updated
to
Z/IP about br-lan
@A.E.M
Logs are:
|
Jul 29 2020, 10:35 AM |
|
Updated
to
Z/IP about br-lan
@A.E.M
254380 DHCP pass completed 357217 IP addresses: |
Jul 29 2020, 10:32 AM |
|
Replied
to
Z/IP about br-lan
@A.E.M
|
Jul 29 2020, 10:30 AM |