Member | Action | Date |
---|---|---|
|
Posted
HOW LONG IT TAKE TO SWITCH FROM TX TO RX IN SI4463. on
Proprietary Wireless Forum
HELLO. I have one remote and One controller. It takes about 40 ms to send out data from Remote to controller. and the controller send out feedback data delayed for 5 ms after received the data from remote. the remote start RX after sending out data. so there is 5 ms gap time for remote and controller to read feedback data. But it fail. remote can not get the data. and the controller really send out the feedback data.
//CODE of REMTOTE. . IF DONE TX . 。Int flag . and enable feedback then startRX. if(Sflag&SI4463_ST_TXDNE)
//Controller. //read an package from device.
else { //start rx again }
|
16 days ago |
|
Posted
How to set the RF Parameters of SI4463 on
Proprietary Wireless Forum
HI . I want to get a good performance of SI4463 communication. The setting attached now reach to 300 meters. what can i change to get longer distance.? It shall be compatible with the setting in use. |
16 days ago |