Member | Action | Date |
---|---|---|
|
Posted
the lifetime of si1153 on
Forum
I want to know the lifetime of the Si1153, 5 years or 10 years? |
Oct 28 2017, 5:37 PM |
|
Posted
si1153贴片生产回流焊温度和时间控制 on
Forum
si1153在STM生产时,回流焊的温度和时间要如何控制,有这方面的指导手册吗 |
Oct 28 2017, 5:37 PM |
|
Posted
si1153接近检测自动工作模式设置门限值 on
Forum
si1153用做接近检测,工作在自动工作模式,设置门限值,但是测量结果,没有超过门限值,也会产生中断。我想实现在自动工作模式,只有测量结果超过门限值才会产生中断,但是参数不管如何设置都不行,请问有什么办法呢? |
Oct 28 2017, 5:37 PM |
|
Posted
the toolchain of EFM8 in simplicity studio on
Forum
I have installed the simplicity studio which version is V4, I want to complier the program based EFM8, now I haved installed the 8051SDK, the console of simplicity studio prompt there is no toolchain. the simplicity studio only support keil c51 as toolchain? |
Oct 28 2017, 5:25 PM |
|
Posted
Delete project from simplicity studio and import project into simplicity studio on
Forum
Delete project from simplicity studio and import project into simplicity studio
Show more
|
Oct 28 2017, 5:19 PM |
|
Posted
unpatch of si4463 which reversion is B1B and C2A on
Forum
The Si4463 has two reversion,one is B1B the other is C2A. when we generated project from WDS, it will include a patch file by default. the si4463 must not patched based version B1B and C2A. in the radio config file, you should change statement below : to below: that is to say: you should alter 0x81 to 0x01. |
Oct 28 2017, 2:55 PM |
|
Posted
在simplicity studio生成工程文件,然后在IAR IDE进行编译 on
Forum
在simplicity studio生成工程文件,然后在IAR IDE进行编译
Show more
|
Oct 28 2017, 2:57 PM |