Member | Action | Date |
---|---|---|
|
Replied
to
EFM8 Sleepy Bee Energy Profiler not working even for demos
I agree that it is weird, that is why I haven't counted this as an answered question. Any suggestions for next steps or more information needed from me? Thanks, Steve |
16 days ago |
|
Replied
to
EFM8 Sleepy Bee Energy Profiler not working even for demos
Okay, so maybe this product doesn't have that feature. When I choose the demo and the demo code there are not Mode options: |
16 days ago |
|
Posted
EFM8 Sleepy Bee Energy Profiler not working even for demos on
8-bit MCU - Microcontroller Forum
I'm using Simplicity Studio Version SV4.1.14.0, and I have the EFM8SB10F8G Starter Kit (SLSTK2010A) When I use Energy Profiler to the MCU current consumption, the code on MCU does not run. When I run in either debug more or standard mode the code runs fine. I am choosing to just run the demo code as is and nothing works in the energy profiler. When I press the reset or the push buttons the Energy profiler shows the current changing but the MCU does not appear to be running code. Can anyone help me with this? Thanks, Steve |
20 days ago |