Member | Action | Date |
---|---|---|
![]() |
Replied
to
Is it possible to have/install two independent versions of Simplicity Studio on the same PC ?
Dear Jim,
Show more
Many thanks for the prompt answer. I have followed your instructions and successfully installed second instance of SSv4 , intended for BLE webinar during May. Thanks and Best regards, |
May 08 2020, 4:18 PM |
![]() |
Selected an answer for
Is it possible to have/install two independent versions of Simplicity Studio on the same PC ?
Yes @bmiseBUCK, By default if the installer is run again a new instance of Simplicity Studio will be installed. The default installation directory will have '_2' appended to it. The trick is that each installation should use it's own workspace, so the existing installation should be changed to use a different workspace than the default one before doing the second installation. Use the [File] > [Switch Workspace] > [Other...] command to create and switch to the new workspace. Simplicity Studio will restart using the new workspace. You can name the workspaces based on the intended use of each instance of Simplicity Studio. Let me know if you have any questions. Thank you, jpitt |
May 08 2020, 4:16 PM |
![]() |
Voted up yes_bmisebuck_bydefaultiftheinstallerisru-oy6s Show more |
May 08 2020, 4:15 PM |
![]() |
Voted up yes_bmisebuck_bydefaultiftheinstallerisru-oy6s Show more |
May 08 2020, 4:15 PM |
![]() |
Voted up yes_bmisebuck_bydefaultiftheinstallerisru-oy6s Show more |
May 08 2020, 4:15 PM |
![]() |
Replied
to
Is it possible to have/install two independent versions of Simplicity Studio on the same PC ?
Many thanks Pit!
Show more
|
May 08 2020, 4:15 PM |
![]() |
Posted
Is it possible to have/install two independent versions of Simplicity Studio on the same PC ? on
Simplicity Studio Forum
Is it possible to have/install two independent versions of Simplicity Studio on the same PC ?
Show more
|
May 08 2020, 11:59 AM |
![]() |
Posted
Adapter IF Invalid Parameter e.g. the serial number may be wrong on
Forum
A few years we have been using successfully a DEBUGADPTR1-USB (USB debug Adapter from SILABS) with our own designed Boards, Simplicity Studio v4, under Windows 7 Target was , usually C8051F380. Now, after installing latest Simplicity Studio v4 to my new PC with Windows10 and new INTEL i9-9400 CPU, installation of SS v4 looks OK, but, with same USB debug Adapter, I CAN NOT start DEBUG session with message : "Adapter IF Invalid Parameter e.g. the serial number may be wrong " Please help !
|
Aug 14 2019, 1:17 PM |
![]() |
Replied
to
Serial adapter(EC2) C2 problem
Thanks, Erik ! |
Oct 28 2017, 1:11 PM |
![]() |
Posted
Serial adapter(EC2) C2 problem on
Forum
I have older Version of C8051F120DK dev. Kit with Serial Adapter EC2... |
Oct 28 2017, 1:11 PM |