Member | Action | Date |
---|---|---|
|
Replied
to
simple periodic timer
In this case LED toggling trough ISR is just an example to check the TIMER0 timings easily and only for debugging purposes. regards, |
Jan 06 2021, 9:39 AM |
|
Selected an answer for
not possible to set email notifications
I can see the same issue as you see in // Community // Settings. Basically, you only need to click the "follow" button and select "Notifications/Email Subscriptions" on the forum/post that you want to follow to get email notification. |
Jan 04 2021, 8:30 AM |
|
Replied
to
simple periodic timer
Oh yes, I've already explored Silabs github site (in my case for series 2). There I've found lot of timer examples (using DMA, to measure period, PWM timer, input capture and so on...) but no one with a simple periodic timer & ISR implementation. regards, |
Jan 03 2021, 6:30 PM |
|
Selected an answer for
Cannot run soc_thermometer example
Basically, BLE examples use bootloader so they can support OAD (over the air download) feature.
Show more
|
Jan 03 2021, 5:55 PM |
|
Selected an answer for
What does "Confirm Firmware" dialog means after starting a debug session?
“SE” stands for security elements which provide some security features such as secure debug interface and secure boot.
Show more
|
Jan 03 2021, 5:53 PM |
|
Replied
to
simple periodic timer
Hi yef, Thank you but actually I haven't much time to learn handler timers with ISR as you suggested. I prefer to expect some support from Silabs as it is a type of sample / demo widely provided by SDKs of other companies. At least with other SDKs that I usually work with (NXP, ST, TI ...) regards, |
Jan 03 2021, 5:52 PM |
|
Updated
to
not possible to set email notifications
I'll give you more details. Here's my notification configuration view with the current Web settings. So far everything is okay. Email settings show all options disabled Next step: Change all the options to 'Yes' and Save
Saved. Everything seems to be okay But not... When I logout and login back the Email notifications remain disabled. In fact I have not received any notification of your reply. This is not a spam issue. regards, |
Jan 03 2021, 5:35 PM |
|
Replied
to
not possible to set email notifications
I'll give you more details. Here's my notification configuration view with the current Web settings. So far everything is okay. Email settings shows all options disabled Next step: Change all the options to 'Yes' and Save
Saved. Everything seems to be okay But no... When I logout and login back the Email notifications remain disabled. In fact I have not received any notification of your reply. This is not a spam issue. regards, |
Jan 03 2021, 5:35 PM |
|
Posted
not possible to set email notifications on
General Interest Forum
Hi, I'm trying to set the forum email notifications with no success. I'm able to change the YES/NO options and also SAVE these changes... but the changes are not saved at all and at the end I not receive any notifications on replies, comments, votes and so on. Please, could anyone help me with this issue? regards, |
Jan 02 2021, 7:38 PM |
|
Posted
simple periodic timer on
32-bit MCU - Microcontroller Forum
Hi, I'd need to implement on my BRD4184A (EFR32BG22) a simple periodic timer (i.e. TIMER0) to toggle one LED through ISR every 1ms? I was digging into many examples but I'm not able to find it. Could anyone give me a hint? regards, |
Jan 02 2021, 7:22 PM |