Member | Action | Date |
---|---|---|
|
Selected an answer for
CP2110 does work ONLY when connected to MacBook via USB hub
Hey Quyen, all good, it was a wrong resistor. Works good now! 👍 Thanks, |
3 days ago |
|
Replied
to
CP2110 does work ONLY when connected to MacBook via USB hub
Hey Quyen, all good, it was a wrong resistor. Works good now! 👍 Thanks, |
3 days ago |
|
Replied
to
CP2110 does work ONLY when connected to MacBook via USB hub
Hey Quyen, Is there a chance that Thunderbolt (Apple's superset of USB-C) has some specifics in regards of connecting Silabs CP2110 compared to standard USB-C specification? Many thanks, Tom |
4 days ago |
|
Replied
to
CP2110 does work ONLY when connected to MacBook via USB hub
Hey Quyen, Thanks for your reply!
Thank you, Tomas |
7 days ago |
|
Posted
CP2110 does work ONLY when connected to MacBook via USB hub on
Interface Device Forum
Hello, I would like to ask for help. I am using CP2110 and USB-C connector on my device. All works great on Mac if it is connected via a USB hub and the LED turns ON. However, the device is not recognized by MacBook when connected directly to the very same USB-C port as was used to connect the USB hub — the LED stays OFF. Is there some specific CP2110 guidance or configuration for USB-C or devices using USB 3.1 or USB 3.0?
Any idea how might we make it work connected directly to Mac (without a USB hub)? P.S. Attaching my system report screenshots to compare how it looks when connected via USB Hub or directly. Many thanks in advance, Tom |
8 days ago |
|
Replied
to
Would it work to pair USB bridge CP2110 and Si1153 sensor?
ok, thanks, Tony!
Show more
|
15 days ago |
|
Selected an answer for
Would it work to pair USB bridge CP2110 and Si1153 sensor?
I don't think that would work.
Show more
|
15 days ago |
|
Updated
to
Would it work to pair USB bridge CP2110 and Si1153 sensor?
Hey Tony, I don't have MCU. Could it be somehow emulated / workarounded using CP2110's UART? Thank you, |
21 days ago |
|
Replied
to
Would it work to pair USB bridge CP2110 and Si1153 sensor?
Hey Tony, I don't. Could it be somehow emulated / workarounded using CP2110's UART? Thank you, |
21 days ago |
|
Updated
to
Would it work to pair USB bridge CP2110 and Si1153 sensor?
Hey Tony, I don't have MCU. Could it be somehow emulated / workaround using CP2110's UART? Thank you, |
21 days ago |