Member | Action | Date | ||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Replied
to
WGM160P Certification Testing (using an example application provided in Gecko OS SDK)
Gecko OS 4.2.5 has been released on 6 Nov 2020, it updated wifi_test.cw.tx_power syntax usage, now it is dbm instead of a quarter of dbm
|
Nov 11 2020, 7:57 AM |
||||||||||
|
Replied
to
Gecko OS Studio 1.0.3 Release Note
Known issue when updating to GSS 1.0.3 |
Oct 21 2020, 8:40 AM |
||||||||||
|
Replied
to
Softap issue on amw037 gecko 2.2 & 2.3
Hi DL, For stream issue, you can poll server before writing to it because server might close connection. see stream_poll I cannot reproduce issue about netmask 192.168.4.x. How often this issue happen? can you try someother devices like windows or iOS. Can you try to update to latest firmware 2.3.1 that recently released (update command: dfu_update -b 2.3.1) For faster response, please create a support ticket at: https://siliconlabs.force.com/s/contactsupport#sort=relevancy Thanks, Manh |
Jul 16 2020, 9:32 AM |
||||||||||
|
Replied
to
Softap issue on amw037 gecko 2.2 & 2.3
Hi DL, Before running setup_web you can set IP range your own by following command:
One more question, what version did you have this issue? We're trying to reproduce this but not success. Thanks, Manh |
Jul 14 2020, 4:54 AM |
||||||||||
|
Replied
to
WGM160P FW update - confirmation of the end of the process
Hi Krzysztof, In the next gos version (4.2.4), the DFU will return a status message in machine mode "DFU Status: <code>" look like:
You can see the dfu status returned code here Please be informed. You can prepare the host for waiting that message. |
Jul 14 2020, 2:36 AM |
||||||||||
|
Updated
to
How to re-direct log into Zentri DMS console ?
Hi Jacson, Answer is YES, you have to claim device to DMS and dont forget these settings: set dms.auto_start_enabled 1 set dms.cmd.enabled 1 Manh |
Jul 07 2020, 3:25 AM |
||||||||||
|
Replied
to
How to re-direct log into Zentri DMS console ?
Hi Jacson, Answer is YES, you have to claim device to DMS and dont forget set dms.auto_start_enabled 1 Manh |
Jul 07 2020, 3:18 AM |
||||||||||
|
Updated
to
How to include external files
hi Pascal, You can try ls to see the files is loaded or not. Another way is using setup web to load file to file system. thanks, Manh |
Jul 04 2020, 4:12 AM |
||||||||||
|
Replied
to
How to include external files
hi Pascal, You can try ls to see the files is loaded or not. Another way is using setup web to load file to file system. thanks, Manh |
Jul 04 2020, 4:11 AM |
||||||||||
|
Replied
to
How to include external files
Hi, Did you edit the .mk file in your project home directory, add a line $(NAME)_RESOURCE_MANIFEST_PATH := resources/manifest.cfg then edit manifest.cfg points to correct files name. You can see a reference by looking to dps_demo https://docs.silabs.com/gecko-os/4/standard/latest/sdk/examples/cloud/dps_demo
Thanks, Manh |
Jul 03 2020, 10:35 AM |