Member | Action | Date |
---|---|---|
|
Replied
to
Controller RF OTA not upgrade from 7.11 to 7.15
Hello Jiehul, Thanks for the response. Using our Gateway Host. zipgateway build version 7.11 then OTA(Over the Air) performed well and z-wave module version updated from 7.11 to 7.12. CASE 2 : zipgateway build version 7.15 then OTA(Over the Air) performed well and z-wave module version not updated from 7.12/7.11 to 7.15. Thanks & Regards,
|
14 days ago |
|
Updated
to
Controller RF OTA not upgrade from 7.11 to 7.15
Hello Jiehui, Thanks for the response. Using our Gateway Host. zipgateway build version 7.11 then OTA(Over the Air) performed well and z-wave module version updated from 7.11 to 7.12. CASE 2 : zipgateway build version 7.15 then OTA(Over the Air) performed well and z-wave module version not updated from 7.12/7.11 to 7.15. Thanks & Regards,
|
14 days ago |
|
Posted
Controller RF OTA not upgrade from 7.11 to 7.15 on
Z-Wave Wireless Forum
Hello Silab, I have a Host processor and on top of the Z-Wave controller, a module shield inserted. Z-wave controller perfectly initializes network with 7.11 and after I do RF OTA of ZW_SerialAPI_Controller_7.15.1_178_ZGM130S_REGION_US.gbl. So, RF OTA has successfully done but after Reboot the (Host) system, zip gateway, and network initialize with 7.11 version only. Not upgrade 7.15 version. Kindly tell me what is the reason behind this? also, tell me up-gradation directly possible from 7.11 to 7.15 or we need to upgrade step by step like 7.11..12...13 so on. if step by step possible then please provide me sample .gbl files with all OTA versions from 7.11 to 7.15. So I will demonstrate on your given files. also, I was trying RF OTA using PC Controller then give it Error - "firmware update locally not supported". Please find attached a screenshot. Thank you. Regards, Pratik J Panchal |
18 days ago |
|
Posted
Zipgateway network initialization issue on
Z-Wave Wireless Forum
Hello, I'm working on Gateway custom board and specification of the board are as follow : Zwave module placed on the Gateway custom board. I was reboot the Gateway device but still the same issue happens. Currently, I'm finding the root cause of this issue I've not any solution regarding this issue. Please find below zipgateway logs and provide me some solution as soon as possible : root@centauri-imx6ull:~# zipgateway Thanks and Regards, |
43 days ago |
|
Posted
Provide support of CO,SMOKE and System Notification support in Z-wave-700 on
Z-Wave Wireless Forum
Hello,
But Instead of providing an individual Add_Notification() function in State_manager, Is there any way to provide in single calling Add_Notification() function. |
Dec 07 2020, 10:21 AM |