Member | Action | Date |
---|---|---|
|
Replied
to
si5342 dynamically set input and/or ouput frequency
Hi Segar,
Thanks for the answer Do you have the source code of FOTF so I can build it for my target? (Linux on arm64)? Or do you have an algorithm how to calculate all the values?
Thanks
Avner
|
Jan 28 2021, 8:13 AM |
|
Posted
si5342 dynamically set input and/or ouput frequency on
Clock Generator, Buffer, Crystal Oscillator Forum
We are using si5342, the input frequency is determined by incoming data, and so is the output frequency. I prefer not to use ClockBuilder Pro and create all the options - since there are many. Is there a way to calculate all the registers' values and set them on run time? We don't mind doing a soft reset or other procedure to make the effect. Thanks |
Jan 27 2021, 2:55 PM |