The Project board is for sharing projects based on Silicon Labs' component with other community members. View Projects Guidelines ›

Hi everyone, I have a project using Arm cortex A53 ( zyngq MP SOC Ultra+), using Xilinx SDK 2017.4, Ucos III repository 1.43.
My device work well, and i try to use file system to read/write data to emmc, but after i use a funtion in StanderLone Library ( xilffs  file system lib, i have just used f_open  fution). the system tick timer interupts donot work, i call funtion OSTimeGet the counter doesnot increase, i check the interupt handler UCOS_TmrTickHandler() it doesnot call after i use the xilffs funtion. i get this bug for the second time, the first when i use funtion sleep() ( a basic funtion in xilinx lib). 

i try to use the other lib system file like ucos-fs but i dont see any example for xilinx, do the ucos-fs is supported with xilinx?

Anyone can help me plz. thanks so much.

  • Projects