I’ve been playing with this great new board for a few days now. One issue I have run into is that the battery life is very poor. I’m only getting a couple of days out of a coin cell.
I’ve dug into the code, and a couple of things become clear. First, when running rom battery, when you connect to the board, all the sensors switch on, and stay on, until you disconnect.
Second, when you read the sensor values, you aren’t reading the sensors directly, you are reading a cached copy of the values, which are updated every 3 seconds, continuously while you are connected - irrespective of how often you actually read the values out.
Thirdly, on USB power, sensors are powered on all the time (OK, not a big deal).
The conclusion is that if you connect, stay connected, and read the sensors once per minute, the sensors are live all the time, and the battery dies quickly. In fact, I’m not sure the device sleeps at all when connected.
If you connect, read, then disconnect, you have the problem that the device times out after 30 seconds (ie goes into deep sleep, and can only be woken with a button push).
I have changed this timeout to 1 hour, reduced the advertising cycle to 500ms (from 100ms) and reduced the led flashes (during advertising) to 20ms every 10 seconds, but the battery life is still poor when connecting, reading, disconnecting once every minute. I’m just reading the environmental sensors.
It seems that although the sensors are off when not connected, the device does not sleep at all when advertising. (Although debug output does say BLE sleep mode enabled).
Does anyone have any suggestions on how to reduce battery drain? Make the device sleep between advertisements? Or any other way to extend the battery life beyond a few days?
This project isn't really an end in itself, just a simple tool for working with the WGM110 Wi-Fi module, but it was suggested that I share it here, so I'm re-posting.
Sometimes it's useful to be able to pre-program modules before they're installed on a board, particularly if your board doesn't have space for a SWD header. The earliest versions of the WGM110 also had a defective DFU bootloader (stop bits were 1/2 bit time) that wouldn't work with some hosts, which made in-circuit programming difficult without SWD.
To address this I made a quick and dirty programming fixture for about $15. The components are a Mill-Max 854-22-010-40-001101 0.050" pitch 10-position pogo pin header to connect to the WGM110, a Samtec SFSD-10-28-H-05.00-SR cable with 20-pin 0.050" pitch plug for the JTAG side, some heat shrink tubing, and a 3D printed holder that I whipped up in Alibre.
This is not really the right JTAG connector - its polarity key is in the wrong place and it's latching - but it's the closest thing that Digi-Key happened to have in stock that had discrete wires. It fits on the dev board as is, and it'll fit on a P&E Cyclone's shrouded header if you snip off the key.
In the orientation shown in the top view photo, the pogo pins are wired to the following JTAG pins:
3 (ground)
(nc)
1 (VDD)
10 (Reset)
(nc)
2 (SWDIO)
4 (SWCLK)
(nc)
(nc)
(nc)
If I was going to be using this much I'd have machined mine from Delrin or anti-static ABS, but for only doing a few dozen units at most it didn't seem worth firing up a milling machine.
Without the holder piece, I can use the pogo pin plug to re-flash modules in circuit that have been bricked by DFU failures. This depends on having the PCB lands extend far enough beyond the periphery of the module to make contact. If you followed the recommended layout in the datasheet, it ought to work. I wouldn't want to have to do many boards this way without an alignment jig to hold it in place, but it works fine to just hold it in place if you're just fixing an occasional mistake and not doing production quantities.
Top view:
Bottom view, with wiring to pogo pins:
The STL file and original model in Alibre format are attached. Keep in mind that I set the dimensions to make it work with my own 3D printer and the fit may require tweaking on yours.
It's no substitute for a proper in-circuit programming setup for production, but it's handy for prototyping and I figured I'd share it here in case anyone else needs such a gadget.
This project isn't really an end in itself, just a simple tool for working with the WGM110 Wi-Fi module, but it was suggested that I share it here, so I'm re-posting.
Sometimes it's useful to be able to pre-program modules before they're installed on a board, particularly if your board doesn't have space for a SWD header. The earliest versions of the WGM110 also had a defective DFU bootloader (stop bits were 1/2 bit time) that wouldn't work with some hosts, which made in-circuit programming difficult without SWD.
To address this I made a quick and dirty programming fixture for about $15. The components are a Mill-Max 854-22-010-40-001101 0.050" pitch 10-position pogo pin header to connect to the WGM110, a Samtec SFSD-10-28-H-05.00-SR cable with 20-pin 0.050" pitch plug for the JTAG side, some heat shrink tubing, and a 3D printed holder that I whipped up in Alibre.
This is not really the right JTAG connector - its polarity key is in the wrong place and it's latching - but it's the closest thing that Digi-Key happened to have in stock that had discrete wires. It fits on the dev board as is, and it'll fit on a P&E Cyclone's shrouded header if you snip off the key.
In the orientation shown in the top view photo, the pogo pins are wired to the following JTAG pins:
3 (ground)
(nc)
1 (VDD)
10 (Reset)
(nc)
2 (SWDIO)
4 (SWCLK)
(nc)
(nc)
(nc)
If I was going to be using this much I'd have machined mine from Delrin or anti-static ABS, but for only doing a few dozen units at most it didn't seem worth firing up a milling machine.
Without the holder piece, I can use the pogo pin plug to re-flash modules in circuit that have been bricked by DFU failures. This depends on having the PCB lands extend far enough beyond the periphery of the module to make contact. If you followed the recommended layout in the datasheet, it ought to work. I wouldn't want to have to do many boards this way without an alignment jig to hold it in place, but it works fine to just hold it in place if you're just fixing an occasional mistake and not doing production quantities.
Top view:
Bottom view, with wiring to pogo pins:
The STL file and original model in Alibre format are attached. Keep in mind that I set the dimensions to make it work with my own 3D printer and the fit may require tweaking on yours.
It's no substitute for a proper in-circuit programming setup for production, but it's handy for prototyping and I figured I'd share it here in case anyone else needs such a gadget.
Projects
Thunderboard Sense Battery Life
I’ve dug into the code, and a couple of things become clear. First, when running rom battery, when you connect to the board, all the sensors switch on, and stay on, until you disconnect.
Second, when you read the sensor values, you aren’t reading the sensors directly, you are reading a cached copy of the values, which are updated every 3 seconds, continuously while you are connected - irrespective of how often you actually read the values out.
Thirdly, on USB power, sensors are powered on all the time (OK, not a big deal).
The conclusion is that if you connect, stay connected, and read the sensors once per minute, the sensors are live all the time, and the battery dies quickly. In fact, I’m not sure the device sleeps at all when connected.
If you connect, read, then disconnect, you have the problem that the device times out after 30 seconds (ie goes into deep sleep, and can only be woken with a button push).
I have changed this timeout to 1 hour, reduced the advertising cycle to 500ms (from 100ms) and reduced the led flashes (during advertising) to 20ms every 10 seconds, but the battery life is still poor when connecting, reading, disconnecting once every minute. I’m just reading the environmental sensors.
It seems that although the sensors are off when not connected, the device does not sleep at all when advertising. (Although debug output does say BLE sleep mode enabled).
Does anyone have any suggestions on how to reduce battery drain? Make the device sleep between advertisements? Or any other way to extend the battery life beyond a few days?
Thanks.
Simple WGM110 programming fixture
This project isn't really an end in itself, just a simple tool for working with the WGM110 Wi-Fi module, but it was suggested that I share it here, so I'm re-posting.
Sometimes it's useful to be able to pre-program modules before they're installed on a board, particularly if your board doesn't have space for a SWD header. The earliest versions of the WGM110 also had a defective DFU bootloader (stop bits were 1/2 bit time) that wouldn't work with some hosts, which made in-circuit programming difficult without SWD.
To address this I made a quick and dirty programming fixture for about $15. The components are a Mill-Max 854-22-010-40-001101 0.050" pitch 10-position pogo pin header to connect to the WGM110, a Samtec SFSD-10-28-H-05.00-SR cable with 20-pin 0.050" pitch plug for the JTAG side, some heat shrink tubing, and a 3D printed holder that I whipped up in Alibre.
This is not really the right JTAG connector - its polarity key is in the wrong place and it's latching - but it's the closest thing that Digi-Key happened to have in stock that had discrete wires. It fits on the dev board as is, and it'll fit on a P&E Cyclone's shrouded header if you snip off the key.
In the orientation shown in the top view photo, the pogo pins are wired to the following JTAG pins:
If I was going to be using this much I'd have machined mine from Delrin or anti-static ABS, but for only doing a few dozen units at most it didn't seem worth firing up a milling machine.
Without the holder piece, I can use the pogo pin plug to re-flash modules in circuit that have been bricked by DFU failures. This depends on having the PCB lands extend far enough beyond the periphery of the module to make contact. If you followed the recommended layout in the datasheet, it ought to work. I wouldn't want to have to do many boards this way without an alignment jig to hold it in place, but it works fine to just hold it in place if you're just fixing an occasional mistake and not doing production quantities.
Top view:
Bottom view, with wiring to pogo pins:
The STL file and original model in Alibre format are attached. Keep in mind that I set the dimensions to make it work with my own 3D printer and the fit may require tweaking on yours.
It's no substitute for a proper in-circuit programming setup for production, but it's handy for prototyping and I figured I'd share it here in case anyone else needs such a gadget.
Scott
Simple WGM110 programming fixture
This project isn't really an end in itself, just a simple tool for working with the WGM110 Wi-Fi module, but it was suggested that I share it here, so I'm re-posting.
Sometimes it's useful to be able to pre-program modules before they're installed on a board, particularly if your board doesn't have space for a SWD header. The earliest versions of the WGM110 also had a defective DFU bootloader (stop bits were 1/2 bit time) that wouldn't work with some hosts, which made in-circuit programming difficult without SWD.
To address this I made a quick and dirty programming fixture for about $15. The components are a Mill-Max 854-22-010-40-001101 0.050" pitch 10-position pogo pin header to connect to the WGM110, a Samtec SFSD-10-28-H-05.00-SR cable with 20-pin 0.050" pitch plug for the JTAG side, some heat shrink tubing, and a 3D printed holder that I whipped up in Alibre.
This is not really the right JTAG connector - its polarity key is in the wrong place and it's latching - but it's the closest thing that Digi-Key happened to have in stock that had discrete wires. It fits on the dev board as is, and it'll fit on a P&E Cyclone's shrouded header if you snip off the key.
In the orientation shown in the top view photo, the pogo pins are wired to the following JTAG pins:
If I was going to be using this much I'd have machined mine from Delrin or anti-static ABS, but for only doing a few dozen units at most it didn't seem worth firing up a milling machine.
Without the holder piece, I can use the pogo pin plug to re-flash modules in circuit that have been bricked by DFU failures. This depends on having the PCB lands extend far enough beyond the periphery of the module to make contact. If you followed the recommended layout in the datasheet, it ought to work. I wouldn't want to have to do many boards this way without an alignment jig to hold it in place, but it works fine to just hold it in place if you're just fixing an occasional mistake and not doing production quantities.
Top view:
Bottom view, with wiring to pogo pins:
The STL file and original model in Alibre format are attached. Keep in mind that I set the dimensions to make it work with my own 3D printer and the fit may require tweaking on yours.
It's no substitute for a proper in-circuit programming setup for production, but it's handy for prototyping and I figured I'd share it here in case anyone else needs such a gadget.
Scott