The Si1133/5x Optical Sensor EXP board now has an example project running on EFM32PG12 MCU to demonstrate our latest Si1153 for proximity/ambient light sensing and Si1133 for UV sensing. The example project will require an EFM32™ Pearl Gecko PG12 Starter Kit(SLSTK3402A) to plug in the Si1133/5x Optical Sensor EXP board through the 20pin expansion header.
The source code of the example project is provided in the attachment.
We also have a nice video describing all the features included in the demo. Please make sure to check it out before getting started.
Is there an example project working with the Si1133/5x-OPT-EXP evaluation board on 8bit MCU? If so, where can I get it?
Answer
The only example project we have for Si1133/5x-OPT-EXP evaluation board is built on the EFM8 BusyBee STK. You can download it in the attachment. The project can be imported into the Simplicity Studio v4. For any project related questions, please submit support tickets to the 8-bit MCU support team.
Sensors Knowledge Base
KBA_SENS_0602: Si1133/Si115x Optical Sensor Example Project on 32bit MCU
The Si1133/5x Optical Sensor EXP board now has an example project running on EFM32PG12 MCU to demonstrate our latest Si1153 for proximity/ambient light sensing and Si1133 for UV sensing. The example project will require an EFM32™ Pearl Gecko PG12 Starter Kit(SLSTK3402A) to plug in the Si1133/5x Optical Sensor EXP board through the 20pin expansion header.
The source code of the example project is provided in the attachment.
We also have a nice video describing all the features included in the demo. Please make sure to check it out before getting started.
KBA_SENS_0605: Si1133/Si115x Optical Sensor EXP Board Example Project on 8bit MCU
Question
Is there an example project working with the Si1133/5x-OPT-EXP evaluation board on 8bit MCU? If so, where can I get it?
Answer
The only example project we have for Si1133/5x-OPT-EXP evaluation board is built on the EFM8 BusyBee STK. You can download it in the attachment. The project can be imported into the Simplicity Studio v4. For any project related questions, please submit support tickets to the 8-bit MCU support team.