Question

Is it possible to change a project's device after it is created?

Answer

Yes, you can change the device that the project is configured for by opening the Properties of the project you want to change. Under C/C++ Build -> Board/Part/SDK, there is an option to change the Boards and then Part fields for that particular project.

  • 8-bit MCUs
  • 32-bit MCUs
  • Development Environments
  • Knowledge Base Articles
  • Simplicity Studio