To enable the debug console window in studio, add the following flag to the top of your studio.ini file, or call studio.exe with the following parameter:

 

 

-consoleLog

This displays a debug console window that shows the real-time output of Studio's status messages. Most of this information is also displayed in the Error Log view.

 

 

consoleLog.png

 

  • Development Environments
  • Knowledge Base Articles
  • Simplicity Studio
  •  Good day I would like to know if the debugger P & E micro is compatible with silmplicity studio V4

    0