The Thunderboard Forum is no longer active. If you would like to post a question regarding Thunderboard Kits, please use the Bluetooth Forum.

Forum

    To receive email updates about this thread, click the Follow button and select Email Subscriptions at the top of the thread page.
    • Android Thunderboard App fails to find any device on Samsung Galaxy A20

      Roya Dibaj | 06/160/2020 | 12:57 PM

      Hi,

      Thunderboard App fails to find SLTB010A or any other SiLabs device on Samsung Galaxy A20. All permissions including the location are given. Please help resolve this issue.

       

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      4
      Replies
      Answered
    • Running AN1186 Mesh Sensor Model in TB Sense 2?

      AdonisReed AdonisReed | 06/163/2020 | 06:49 AM

      Hi there,

       

      I'm trying to run the Mesh example in two boards but I'm getting a "init failed (0x180)" error from both client and server borads. https://snaptube.cam/ 9apps It seems that the upgrade to a the lasta dapter firmware let me there- Is it possible to have the original TB Sense 2 firmware?. Or if you have a clue please help me.

       

      Thanks.

      • Discussion Forums
      • Thunderboard Kits
      1
      Replies
      Unanswered
    • Thunderboard Sense 2 fails to sleep after reset

      Yohannes Tesfai | 05/136/2020 | 04:13 PM

      Hi

      In my application that runs on Thunderboard Sense 2, I was having issues where the tag sometimes goes to EM2 properly and sometimes never goes to EM2 after reset. The issue when it happens is a permanent issue. i.e. when the board powers up or comes out of button reset, EM2 sleep mode either works properly always or never goes to sleep and never recovers until another reset. Upon another reset again sometimes works sometimes doesn't.

      To make sure that it wasn't my application that was causing the issue, I used one of the example projects running on Thunderboard Sense 2 and I am seeing the same unexpected power mode behavior. The project is:

      "SOC Thunderboard Sense"
      Bluetooth: Thunderboard Sense application

      I used Simplicity Studio to create the project as follows:

      - Plug in my Thunderboard Sense 2 through the debugger USB cable
      - Click on J-Link and hit "New Project" Button
      - Select "Bluetooth SDK 2.12.2.0" and click Next
      - Select "SOC - Thunderboard Sense, Bluetooth: Thunderboard Sense application" and click Next
      - Accept default name and click Next
      - Accept the pre populated board (Thunderboard Sense 2 (BRD4166A) and click Finish

      I then connected my Thunderboard Sense 2 to HAPPY GECKO debug board via mini connector cable to measure current consumption. I noticed after powerup/reset, sometimes EM2 sleep works properly and I can see sleep periods, but sometimes sleep is never allowed and board remains in high power (close to 10mA) mode. Please see attached pdf file for a marked up screen capture.

      I also dug into the issue some more and what is happening is that in SLEEP_sleep() function in sleep.c, SLEEP_LowestEnergyModeGet() is always returning EM1 because sleepBlockCnt[sleepEM2-2U] is always > 0 (actually always 2).

      Any help with this issue would be great because battery life is critical to our application and obviously 50/50 chance of never going to low power mode will not work for us.

      Thanks
      Yohannes

      • Discussion Forums
      • 32-bit MCUs
      3
      Replies
      Unanswered
    • Thunderboard BG22 onboard mics

      giovgris | 06/156/2020 | 08:28 AM

      Hi,
      what about the two mics, U7 and U11, of the EFR32BG22 board?
      I don't find anything for the use of it.

      Thanks in advance 

      Giovanni

      • Discussion Forums
      • Thunderboard Kits
      13
      Replies
      Unanswered
    • Layout (Gerber) files for Thunderboard Sense 2

      Yohannes Tesfai | 06/161/2020 | 02:07 PM

      Hi, 

      I found board layout files for the Thunderboard Sense (BRD4160A-A02-pkg) in this community forum. Is there a similar file for Thunderboard Sense 2 (BRD4166A)?

      Thanks

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      2
      Replies
      Answered
    • Thunderboard Sense 2 WiFi

      zageek | 06/161/2020 | 12:32 PM

      Is it possible for the 2.4GHz radio on the Thunderboard Sense 2 to implement WiFi?

      I have received  unit and I like it but it would be convenient to directly access it via WiFi

      • Discussion Forums
      • Thunderboard Kits
      1
      Replies
      Unanswered
    • EMLINK failed - Thunderboard Sense 2 (SLTB004A)

      V V | 05/139/2020 | 12:36 PM

      Hi,

      After a not successful software update, my Thunderboard Sense 2 shows:

      • "EMLINK failed" error when I try to change "Debug Mode" from OFF to MCU.

      There is any way to reset the board?

      Thanks,

      AI

      • Discussion Forums
      • Simplicity Commander
      • Simplicity Studio
      • Thunderboard Kits
      • SLTB004A
      3
      Replies
      Unanswered
    • using Sigfox in Thunderboard Sense 2

      Nabil DRISSI EL BOUZAIDI | 06/153/2020 | 09:11 AM

      Hi!

      I'm currently using Thunderboard snese 2 and I want to send some information throught Sigfox Platform, I already have Wisol SFM10R1 as  Sigfox module,

      I want to know how can I addapte this module with the Tb s2

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      3
      Replies
      Answered
    • Thunderboard or EFR32BG22C222F352GM32 BLE scanning of other BLE or Bluetooth device

      Moumita Kundu | 06/153/2020 | 08:52 AM
      Can thunderboard or EFR32BG22C222F352GM32 ble scan its nearby ble or bluetooth devices with signal  strength? If it can then please guide me with the solutions.
      • Discussion Forums
      • Thunderboard Kits
      1
      Replies
      Unanswered
    • Flash programming the EFM8 (PIC) from the EFR32MG on Thunderboard Sense

      Gary Sugar | 01/29/2020 | 04:17 PM

      Hi - 

      I'm working on a project that uses a Thunderboard Sense PCB, but with a EFR32MG13 instead of the EFR32MG1. Since we'll be building these boards from scratch, I'm looking for a way to program the EFM8 (which is used as a power + interrupt controller (PIC) on the Thunderboard Sense) with the PIC firmware. From looking at the schematic, I can see that the EFR32MG is connected to the EFM8 through the DBG_C2CK and CBG_C2D lines. Does anyone know if there's a way to program the PIC firmware into the EFM8 from the EFR32MG? Can anyone even identify which firmware is used in the EFM8 for the PIC functions?

      Thanks!

      Gary

      • Bluetooth Low Energy
      • Discussion Forums
      • Answered
      • Thunderboard Kits
      1
      Replies
      Answered
    • Thunderboard EFR32BG22 debugging blocked

      Clarck_D | 05/135/2020 | 11:53 AM

      Hi,

      I have trouble debugging my thunderboard. Debugging used to work fine, but now I can see in the dissasembly that it blocks in a loop before I can even launch the program.

      The program don't go further than the beq instruction.

      I've faced a similar problem before and debugging worked fine after I've created a new workspace and used the example program for Bluetooth SDK 2.13.5.0 : SOC - Thunderboard.

       

      Anyway, i've just done a device recover using the command :

      C:\SiliconLabs\SimplicityStudio\v4\developer\adapter_packs\commander device recover

       

      Often, I also have problems when I try to debug and this prompt :

      Most of the time, clicking on the "Click to query Lock Status" doesn't fix the issue. And I tried "Unlock All" even though there is no devices in Preferences->Simplicity Studio-> Adapters Packs-> Device locks.

       

      These problems are annoying and kind of discouraging for new users on this environment like I am :/

       

      More infos on my config :

       

       

       

      • Discussion Forums
      • Thunderboard Kits
      7
      Replies
      Unanswered
    • CR2032 battery longivity with EFR32BG22C222F352GM32​ current consumption while in transmitting mode.

      Moumita Kundu | 05/140/2020 | 04:01 AM

      Hi,

      I have a query regarding the EFR32BG22C222F352GM32​ bluetooth IC. Can you please help me out?
      I am calculating the current consumption f the BLE part only. I am calculating here also and please rectify If I am misunderstanding. 
      EFR32BG22 Tx current @0 dbm output power----- 4.65 mA=4100uA( avg)
      EFR32BG22 Sleep Mode current -----------------------1.30uA (EM2 mode)
      EFR32BG22 Sleep Mode current----------------------- 0.17uA (EM4 mode)
      Battery capacity-------------------------------------------- 225mAh
       
      Situation 1> If IC is always in sleep mode (EM2)
      Toal current consumption/h= 1.3uA
      Total Power Consumption= 1.3uA*3V=3.9uW
      Battery life (with 90%battery efficiency)= {(225mA*1000*3V)/3.9uW}*0.9= 155,769.231h=6490.38DAYS= 17.78 years
       
      Situation 2> If data transmission is done in every hour for 30 secs
      Toal current consumption/h= {(4650*30)/3600}+{(1.3*3570)/3600}=40.039uA
      Total Power Consumption= 40.039uA*3V=120.11uW
      Battery life (with 90%battery efficiency)= {(225mA*1000*3V)/120.11uW}*0.9= 5057.86h=210days
       
      Somewhere I read that using CR2032 battery it will run for 5 years. Am I taking anything wrong? Can you please suggest me how we can minimize the Tx current consumption so that we can use the battery atleast for 1 year? We will transmit stored data in every 15 minutes.
      • Discussion Forums
      • Thunderboard Kits
      2
      Replies
      Unanswered
    • THunderboard Sense v 2. Where is the Firebase code?

      Ricardo Gutierrez | 08/218/2019 | 01:27 AM

      Hi there,

       

      When I try to check the Firebase code of the Android code base for the board sample, it shows me an error. Does somebody of you know where can I find the code or the replacement to this?

       

      Thanks.

       

      • Discussion Forums
      • Thunderboard Kits
      7
      Replies
      Unanswered
    • Android Thunderboard App fails to find any devices on Android 10

      Daniel Olsson | 05/139/2020 | 06:56 AM

      Hi, I have three devices, one BG22 (SLTB010A) and two sense 2 (SLTB004A) - all running Preflashed FW. All boards show up and report data to IOS Devices and also work fine with an old Samsung Galaxy S4 (android 6) but fail with devices having latest versions of android, specifically Google pixel 3a (out of the box). I tested with the play store version of the app and also tried to build one from the repo but results are the same Galaxy S4 and IOS devices work but Google Pixel 3a does not work.

      Kindly help with this!

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      1
      Replies
      Answered
    • Thunderboard Sense 2 Temp sensor (SI7021)

      R.V. | 03/85/2020 | 08:44 PM

      Whilst working on a project using a thunderboard sense 2, I'm encountering a few problems regarding the onboard temperature sensor

      (The project builds upon the bluetooth soc empty example)

      First I added the following headers to the main.c file (retargetserial used for monitoring output during debugging  )

      Afterwards I added the following code (inspired by the code used in the thunderboard sense 2 example project)

      However, during debugging in simplicity studio the code fails to execute the SI7021_init() function.  

      Terminal output confirms simplicity studio debugger : si7021_init() never executes properly.

      Any suggestion that can help solve this problem? 

      Kind regards,

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      2
      Replies
      Answered