The Thunderboard Forum is no longer active. If you would like to post a question regarding Thunderboard Kits, please use the Bluetooth Forum.

This discussion and its replies are closed

Hallo,

 

I want to add bluetooth communication to my Giant Gecko EFM32 MCU via BGM111 connected via USART and BGLib.

 

Is there an example how to add bglib communiction into EFM32 MCU firmware?

Is bglib implementation ready to usage available for EFM32 giant geckco?

 

best regards
Oliver Rettig

  • Discussion Forums
  • Thunderboard Kits
Unanswered
  • I have the same issue. (Wonder Gecko 3800 + BGM111)

    It is looking for an example source code.

    But i cannot found the thunderboard wear sample code.
    www.silabs.com/thunderboardwear

    0
  • Hi,

     

    Unfortunately there is no host example code for the Geckos.

     

    But the Simplicity C SDK contains NCP examples (target & host project in one) where the host part is quite generic.

    These can be ported to any host including the Geckos.

     

    Cheers,

    Balázs

     

     

    0