Hi,
I am writing a firmware for BGM121 which deals multiple bondings. Bluetooth Software API Reference Manual says that the number of bondings are limited to 14, but its bonding handle ranges from 0 to 31. I want to know whether the bonding handle can be really that big or it cannot be more than 14 or the max_bonding_count set by the sm_store_bonding_configuration command.
Actual range of bonding handle
Hi,
I am writing a firmware for BGM121 which deals multiple bondings. Bluetooth Software API Reference Manual says that the number of bondings are limited to 14, but its bonding handle ranges from 0 to 31. I want to know whether the bonding handle can be really that big or it cannot be more than 14 or the max_bonding_count set by the sm_store_bonding_configuration command.
Thank you for clarifying the situation, tmonte! If the limit is set to default 14, the value of bonding handle remains under 14?