It often happens, that the Bluetooth stack needs to run multiple tasks, that use the radio, at the same time. E.g. you can simultaneously send out advertisements and scan for new devices. You can keep alive multiple connections at the same time. You can initiate a new connection while still scanning for new devices. Actually, you can even initiate a new connection while you are scanning for new devices, you are advertising, and you keep alive an already established connection.
In reality, the stack can only perform one task at a time (even though the tasks appear to run simultaneously). At any given time, the radio can be only configured to do one of the followings:
send a packet, or
receive a packet, or
listen on a channel
Because of this, simultaneous radio tasks need to be prioritized. The radio scheduler will decide the order in which tasks are run based on the priorities.
Default priorities
The Bluetooth stack distinguishes 4 kind of radio tasks:
scanning
advertising
connection initiation
connection maintenance
Scanning: Scanning means listening for advertisement packets on the three advertisement channels and periodically switching the channel. Scanning is a low priority task, since missing a single advertisement is not a serious problem. Other task may need to interrupt scanning at any time, e.g. to keep the connection alive.
Advertising: Advertising means repeatedly sending out advertisement packets. Advertisement is also low priority. Since the exact timing of advertisements are not critical, advertisement packets can be delayed in order to yield the radio for higher priority tasks.
Connection initiation: Connection initiation consists of two steps: scanning to find the advertisement of the device we want to connect to and sending the connection request in the connection request window right after the advertisement. Connection initiation has high priority, since
we want to find the very first advertisement to connect quickly
the connection request needs to be sent accurately in the connection request window
Connection maintenance: Connection maintenance means that the device needs to send at least one packet to the peer device and receive at least one packet from the peer device in every connection interval (if slave latency is defined, then the slave can skip some connection intervals.) These packets need very strict timing, they cannot be delayed, and missing lots of them may lead to connection loss, hence sending/receiving packets on a connection has high priority.
The default priorities for the different tasks are listed here. Note, that every task gets the minimum priority first which can be increased up to the maximum priority during time. This is explained in the next section.
The lowest possible priority is 255 and the highest priority is 0.
task type
min. priority
max. priority
scanning
191
143
advertising
175
127
connection init
55
15
connection
135
0
Dynamic priorities
The Bluetooth stack uses dynamic priorities, which means that every radio task starts with a lower priority, and every time the task fails to be scheduled, its priority increases. This ensures that simultaneous tasks are served fairly. As you saw in the table of the previous section, all four radio task types have a minimum and a maximum priority. By default the task-specific minimum priority is assigned to the tasks, which can be increased up to the task-specific maximum priority. E.g. connections have higher priority than advertisements. But if many advertisement packets were not sent due to connection maintenance, then their priority can raise over the minimum connection priority, and actually for a short time advertisement can have higher priority.
Another example is when multiple connections are open, and their transmit/receive windows overlap. In this case the connection with the highest priority is served. The priority of the served connection drops back to the minimum priority, and the priority of other colliding connections are increased. Hence all connections are served within a reasonable time. The priority is always increased with such rate that it reaches 0 (highest) priority before the supervision timeout. E.g. if you have two connections with 100ms and 10s supervision timeouts respectively, then the priority of the first one increases quickly while the priority of the second one increases slowly. This ensures that all connections are served before their supervision timeout.
The default priorities are chosen so, that they can be used well in most use cases. However, you might have a use case, where the default priorities does not provide an optimal solution. E.g. if in your application it is not important to connect quickly but it is very important to send data in every connection interval via an already established connection, then you can lower the priority of the connection initiation process.
The min. and max. priorities of each task type can be defined in a gecko_bluetooth_ll_priorities structure. If you refer to this structure in the gecko_configuration_t structure, then the default priorities will be overwritten with these values. (Note: the default priorities are defined under GECKO_BLUETOOTH_PRIORITIES_DEFAULT)
threshold_coex is not discussed here. rail_mapping_offset and rail_mapping_range are discussed in the next section.
Priorities in Bluetooth + RAIL DMP application
In a Bluetooth + RAIL DMP application your proprietary protocol also need to use radio priorities. In this case the Bluetooth priorities are mapped to a small range of the RAIL priorities, so that you can define radio tasks with a priority higher than the highest Bluetooth priority and with a priority lower than the lowest Bluetooth priority. By default Bluetooth priorities are mapped to the 16..32 RAIL priority range - meaning that the 0 Bluetooth priority corresponds to RAIL priority 16, and the 255 Bluetooth priority corresponds to RAIL priority 32. This can also be changed in the gecko configuration structure with the last two parameters of the linklayer_priorities. The offset defines the highest RAIL priority (that corresponds to 0 Bluetooth priority) and the range defines the difference between the lowest and highest priority (by default 32 - 16 = 16).
KBA_BT_0407: Bluetooth Radio Task Priorities
It often happens, that the Bluetooth stack needs to run multiple tasks, that use the radio, at the same time. E.g. you can simultaneously send out advertisements and scan for new devices. You can keep alive multiple connections at the same time. You can initiate a new connection while still scanning for new devices. Actually, you can even initiate a new connection while you are scanning for new devices, you are advertising, and you keep alive an already established connection.
In reality, the stack can only perform one task at a time (even though the tasks appear to run simultaneously). At any given time, the radio can be only configured to do one of the followings:
Because of this, simultaneous radio tasks need to be prioritized. The radio scheduler will decide the order in which tasks are run based on the priorities.
Default priorities
The Bluetooth stack distinguishes 4 kind of radio tasks:
Scanning: Scanning means listening for advertisement packets on the three advertisement channels and periodically switching the channel. Scanning is a low priority task, since missing a single advertisement is not a serious problem. Other task may need to interrupt scanning at any time, e.g. to keep the connection alive.
Advertising: Advertising means repeatedly sending out advertisement packets. Advertisement is also low priority. Since the exact timing of advertisements are not critical, advertisement packets can be delayed in order to yield the radio for higher priority tasks.
Connection initiation: Connection initiation consists of two steps: scanning to find the advertisement of the device we want to connect to and sending the connection request in the connection request window right after the advertisement. Connection initiation has high priority, since
Connection maintenance: Connection maintenance means that the device needs to send at least one packet to the peer device and receive at least one packet from the peer device in every connection interval (if slave latency is defined, then the slave can skip some connection intervals.) These packets need very strict timing, they cannot be delayed, and missing lots of them may lead to connection loss, hence sending/receiving packets on a connection has high priority.
The default priorities for the different tasks are listed here. Note, that every task gets the minimum priority first which can be increased up to the maximum priority during time. This is explained in the next section.
The lowest possible priority is 255 and the highest priority is 0.
Dynamic priorities
The Bluetooth stack uses dynamic priorities, which means that every radio task starts with a lower priority, and every time the task fails to be scheduled, its priority increases. This ensures that simultaneous tasks are served fairly. As you saw in the table of the previous section, all four radio task types have a minimum and a maximum priority. By default the task-specific minimum priority is assigned to the tasks, which can be increased up to the task-specific maximum priority. E.g. connections have higher priority than advertisements. But if many advertisement packets were not sent due to connection maintenance, then their priority can raise over the minimum connection priority, and actually for a short time advertisement can have higher priority.
Another example is when multiple connections are open, and their transmit/receive windows overlap. In this case the connection with the highest priority is served. The priority of the served connection drops back to the minimum priority, and the priority of other colliding connections are increased. Hence all connections are served within a reasonable time. The priority is always increased with such rate that it reaches 0 (highest) priority before the supervision timeout. E.g. if you have two connections with 100ms and 10s supervision timeouts respectively, then the priority of the first one increases quickly while the priority of the second one increases slowly. This ensures that all connections are served before their supervision timeout.
For more information about Bluetooth priority handling please refer to UG305: Dynamic Multiprotocol User’s Guide.
Changing priorities
The default priorities are chosen so, that they can be used well in most use cases. However, you might have a use case, where the default priorities does not provide an optimal solution. E.g. if in your application it is not important to connect quickly but it is very important to send data in every connection interval via an already established connection, then you can lower the priority of the connection initiation process.
The min. and max. priorities of each task type can be defined in a
gecko_bluetooth_ll_priorities
structure. If you refer to this structure in thegecko_configuration_t
structure, then the default priorities will be overwritten with these values. (Note: the default priorities are defined underGECKO_BLUETOOTH_PRIORITIES_DEFAULT
)threshold_coex is not discussed here. rail_mapping_offset and rail_mapping_range are discussed in the next section.
Priorities in Bluetooth + RAIL DMP application
In a Bluetooth + RAIL DMP application your proprietary protocol also need to use radio priorities. In this case the Bluetooth priorities are mapped to a small range of the RAIL priorities, so that you can define radio tasks with a priority higher than the highest Bluetooth priority and with a priority lower than the lowest Bluetooth priority. By default Bluetooth priorities are mapped to the 16..32 RAIL priority range - meaning that the 0 Bluetooth priority corresponds to RAIL priority 16, and the 255 Bluetooth priority corresponds to RAIL priority 32. This can also be changed in the gecko configuration structure with the last two parameters of the linklayer_priorities. The offset defines the highest RAIL priority (that corresponds to 0 Bluetooth priority) and the range defines the difference between the lowest and highest priority (by default 32 - 16 = 16).